MOSFET (Si/SiC) Forum Discussions
Good afternoon, can you help me check if the LOT traceability is consistent with the original factory. The complete label of the attachment. The customer told me that the goods have slight scratches.
Hi,
I'm currently creating a design with three different Infineon MOSFETs, all with a slightly different flavor of a PG-TDSON-8 package / footprint.
I'm having trouble interpreting the different drawings contained in the datasheets and the separate footprint drawings. I can't clearly identify PCB copper dimensions, solder mask openings and paste mask / stencil openings. The drawings containing the suggested solder mask & stencil openings don't provide suggested copper dimensions.
Maybe I'm overlooking something or I'm looking at the wrong documents. Can someone give me a hint?
In case of the part number BSC035N04LS G my guess would be that I should design solder mask and stencil openings according to this document, referenced via the package: https://www.infineon.com/cms/en/product/packages/PG-TDSON/PG-TDSON-8-1/#!?fileId=5546d4625cc9456a015cd505df0c2e1b
Copper is shown as shaded areas, but without dimensions.
Thanks in advance for your kind support!
Best regards
Markus
Does Infineon make a rad-hard, n-CH, depletion mode MOSFET, similar to the LND-150? I would like to use it as a current-limiter limiting the current into an ADC. The depletion mode MOSFET is on with VGS = 0 V. They are not as popular as enhancement mode MOSFETs and I'm having a hard time finding a rad-hard one.
Show LessDear all,
I am trying to implement the Dynamic Test Circuit in LTSpice of IMZA120R007M1H_L3. I am facing errors to simulate the circuit. Here i am attaching the test circuit and errors occurring during the simulation.
I hope you can help me fix the model/simulation.
Thank you and kind regards
Show LessHi, May I have the soldering guidelines for the mentioned IRL7486MTRPbF MOSFET? I do not understand how to solder at low temperatures, it took me so much time. That is why I am using High-temperature air like 400 degrees Celsius, but every time I soldered the MOSFET at these temperatures, it is not working. I have only a hot air blower, PCB board heater till 200 degrees C max, and solder paste. It is better if the debugging procedure of MOSFET is also discussed, to avoid soldering mistakes for further functionality. How can I make sure that the MOSFET is soldered properly?
Thanks in advance
We bought IPD60R600P6 2500pcs D/C2307+ from Arrow(pic 5) , but we found there are many scratches and black point (pic1-5), the Arrow told us they are from your craft problem ,but I think they have a affect in the transport process ,especially the black point ,it is oxidation. Now we need return these goods to them ,but they can’t accept . Could you help us these are common chips from you or their problems lead to the oxidation, thanks . Wait your kindly reply soon ,thanks~
Show LessI would like to confirm one point regarding the dimensions of ISC009N06LM5.
Regarding the ISC009N06LM5, the PKG height information is only MAX, but do you know the Typ and Min?
Model number:ISC009N06LM5
https://www.infineon.com/cms/en/product/power/mosfet/n-channel/isc009n06lm5/
Show LessHi Community!
Hope you all are doing great!
I am trying to figure out the model number of this component!
This is used in a stepper motor drive and needs to be replcaed!
By any chance could someone help me identify this device part number through which I can order this?
Any information or ordering link will be helpful!
Thanks and Regards
Show Less