MOSFET (Si/SiC) Forum Discussions
Dear Sir,
We seen the IFX DS of SIC MOSFET have different Vgs spec from different package.
1. can you help us to confirm that following spec? thanks!
IMZA65R027M1H(TO-247)
Vgs.dynamic -5 to +23V@tpulse,negative<15ns, why only negative pulse time in DS?
Vgs.static ?
Vgs.recommended 0 to +18V
IMBG65R030M1H (TO-263)
Vgs.dynamic -7 to +25V@tpulse,positive<1% duty cycle / fs, why only positive pulse time in DS?
Vgs.static ?
Vgs.recommended -2 to +20V, why recommended Vgs use -2V for MOSFET turn off ?
2. Last question is whether Infineon SIC MOSFET has been changed from trench to planar structure?
Show Less
Hi,
I am trying to tune the cascaded PI controller for 3.3kW PFC. The cascaded PI controller has outer voltage Loop and a inner current loop. How should I approach to choose the correct Kp , Ki values for both Loops for different load current and for Input RMS voltage of 200 to 250v.
CASCADED PI CONTROLLER LOOP
Show Less
Please, I need to know the difference between BSC067N06LS3G and BSC067N06LS3GATMA1.
IRL60B216 is discontinued,please help recommend alternative products.
what surface finish is used on these COOLMOS CFD7 mosfets? TIN MATTE? thanks
Hello
您好,我最近在设计一个3KW 400V/54V DCDC LLC,想寻求一些高功率密度和高效率的设计。我在英飞凌的文档中看到了 750W 400KHZ LLC 380V TO 12V 的效率非常高的设计。不,请提供一些参数,非常感谢
关于我找到的文档的标题:Infineon-Presentation_GalliumNitride_AdvancedSiliconDevices-AP-v01_00-EN
Show LessL5 in the dimensional drawing indicates the length of which part of the lead?
I think it is long up to the bulge of the lead.
The dimension L5 > L1-L is also listed as "lead dimension uncontrolled in L5".
Show Less