MOSFET (Si/SiC) Forum Discussions
Hi all,
I'm having trouble deriving how much pulse drain current this HEXFET can handle at 50ms. The graphs on the datasheet seem to be very meshed ink and majority of the pulses are done in the micro-seconds.
What would be the maximum pulse current this transistor can handle at 50ms?
Datasheet attached.
Show LessHi guys,
Just want to understand what is the push factor to develop IPT015N10NF2S. There are competitor in the market like AOS - AOTL66912 which offer cheaper and better spec. How to compete with this part?
Please advise.
Thanks.
Show Less
Good evening, I am a hardware engineer at Lockheed Martin and our customer is requesting for any reliability monitoring qualification data for part numbers IPB65R099CFD7AATMA1 and IPD60R360P7ATMA1 from within 36 months. Our customer sees that the following attached qualification data was qualified since either 2017 or 2020. I am specifically asking about part numbers IPB65R099CFD7AATMA1 and IPD60R360P7ATMA1
Show LessHi Team,
LTspice simulation not working with the spice model provided on the ipw60r060p7 MOSFET design support page of infineon. There is no error displayed in LTspice , the simulation is getting stuck after few microseconds. This is happening with L1 model of ipw60r060p7. The same LTspice simulation is working with IPB65R050CFD7A_L1 model.
Please help to provide correct L1/L3 LTspice models of ipw60r060p7 MOSFET.
Thank you
Show Less
搜索器件IRF220会出现:IRF220PBF、IRF220N、IRF220NPBF的资料,IRF220PBF的资料版本PD-95069A,IRF220N的资料版本PD-94048,IRF220NPBF的资料版本PD-95063A。现有器件标识IRF220, Is this a correct understanding of what the device suffix N means, whether it is the first part without N or the second part with N, and what is the difference between the different suffixes?
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/MOSFET-Si-SiC/MOS%E5%99%A8%E4%BB%B6%E5%B0%BE%E7%BC%80N%E8%A1%A8%E7%A4%BA%E4%BB%80%E4%B9%88%E5%90%AB%E4%B9%89/td-p/492033
Show LessThe use of an IPW65R041CFD7, used to replace the original product in the IPW65R041CFD. in the case of the same drive circuit, IPW65R041CFD7 drive waveform oscillations are obviously more violent (and sometimes break through the damage to the driver chip inside the MOS), the driver chip is close to the MOS alignment is very short and wide (width of 3mm, length of 10mm), and by increasing the drive resistor (from 5Ω to 50Ω), are not obvious effect, is very incomprehensible. And by increasing the drive resistor (from 5Ω to 50Ω), there is no obvious effect, very incomprehensible. I have uploaded a PDF file of the test waveforms in the attachment.
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/MOSFET-Si-SiC/CoolMOS%E7%B3%BB%E5%88%97IPW65R041CFD7%E9%A9%B1%E5%8A%A8%E6%B3%A2%E5%BD%A2%E6%8C%AF%E8%8D%A1-IPW65R041CFD7/td-p/492339
Show Less
Can you please tell me where Figure 30 comes from, is the current drop rate monotonic on the turn-off time?
This is a question asked by a fan in a Zhihu article, please engineer answer~
Link to article is: https: //zhuanlan.zhihu.com/p/403334986
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/MOSFET-Si-SiC/%E7%94%B5%E6%B5%81%E4%B8%8B%E9%99%8D%E7%8E%87%E5%AF%B9%E5%85%B3%E6%96%AD%E6%97%B6%E9%97%B4%E7%9A%84%E5%BD%B1%E5%93%8D%E6%98%AF%E5%8D%95%E8%B0%83%E7%9A%84%E5%90%97/td-p/489318
Show LessLooking for a solar micro inverter solution Infineon PMM-SE1401 complete document
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/MOSFET-Si-SiC/Looking-for-a-solar-micro-inverter-solution-Infineon-PMM-SE1401-complete/td-p/488628
Show LessDoes the IRLML20230TRPBF contain any titanium in the part?