Announcements

Curious on how you can apply MOSFET to Smart Home Appliances? Register for the ASEAN Smart Home Appliance Webinar here to find out how.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

MOSFET (Si/SiC) Forum Discussions

MOSFET (Si/SiC) Forum Discussions

Sort by:
Katholni
MOSFET (Si/SiC)
Hi colleagues ! I can`t find a basictype for  IMZA120R015M1H. We need this for export control classification evidence best regards, Bernhard Show More
Harold
MOSFET (Si/SiC)
I want to use a MOSFET as a switch driven by my microcomputer.     The original circuit using N-channel MOSFET is on the left side. Honestly, I do no... Show More
树暖
MOSFET (Si/SiC)
想挑选一款可用于100M~1GHz高频下进行半波整流的二极管,选用了BAT15-03w,但是未到达所需频段就丧失了整流特性。所以想了解二极管用于半波整流电路对接的负载电阻和输入信号的有什么硬性要求?是否有满足我性能需求的二极管可以推荐?已知输入信号不应超过截止频率,在论文中看到有截止频率应为工作频率... Show More
MS_19060803
MOSFET (Si/SiC)
いつもお世話になっております。 パッケージ(PG-HSOF-8)の内部構造についてご教示いただけないでしょうか。   下記のANのP.5にパッケージ内部が記載されています。 ↓ https://www.infineon.com/dgdl/Infineon-ApplicationNote_650V_CoolMOS_C7_Gold_TOLeadless.pdf-AN-v01_01-EN.pdf?fileId=5546d46253f65057015495adbf15197d... Show More
MS_19060803
MOSFET (Si/SiC)
いつもお世話になっております。 パッケージ(PG-HSOF-8)のパワーサイクル試験のデータ要求がございましので データを取得されていましたら、情報を開示して頂けないでしょうか?   デバイスはIPT030N12N3 Gになります。   また、パッケージ(PG-HSOF-8)よりパワーサイクルの長い... Show More
SoU_4942226
MOSFET (Si/SiC)
いつもお世話になっております。 MOSFETのリード製品の温度測定ポイントをご教示いただけないでしょうか。 下記のANのP.4に記載の内容から裏面の中央が測定位置になると考えていますが認識間違いないでしょうか。 https://www.infineon.com/dgdl/Infineon-Recommendations_for_Board_Assembly_TO-AP-v02_00-EN.pdf?fileId=db3a3043183a955501189e662ae34052... Show More
DJTao
MOSFET (Si/SiC)
  What does each character mean for the six characters on the body? eg. GAT036 on attached picture. Thanks in advance for help   Show More
Harold
MOSFET (Si/SiC)
I'm not sure if I can drive a 24V (0.5A) dc motor with the following circuits?I fear that there will be burned too much power in the transistor when t... Show More
User19686
MOSFET (Si/SiC)
Hello,The package of this component is PG-TDSON-8-33. The Rthja is 50K/W with a 6 cm² cooling area on a one layer 70µm copper PCB.Does anyone know the... Show More
SoU_4942226
MOSFET (Si/SiC)
いつもお世話になっております。TO-220 FullPAK Narrow Leads の実装方法についてご相談させてください。端子の根元部分まで基板穴に挿入して、部品パッケージを基板上に載せた状態(以下の図)で、基板に実装、使用しても問題ないでしょうか? 下記の実装に関するアプリケーションではリード... Show More
Forum Information

MOSFET (Si/SiC)

Power MOSFETs have become an integral part of most of industrial and automotive applications, and Infineon offers leading-edge solutions to suit all needs. Infineon’s innovative OptiMOS™, CoolMOS™, and StrongIRFET™ low and medium voltage power MOSFETs consistently meet the highest quality and performance demands in key specifications for power system design, such as on-state resistance and figure of merit characteristics. Additionally, CoolMOS™ superjunction MOSFET offers a whole host of options for consumer, industrial, and automotive applications such as lighting, TV, audio, server/telecom, solar, EV charging, DC-DC converter, onboard chargers, and many more . In this forum, you can post your questions, comments, and feedback about Si/ SiC MOSFET of both industrial and automotive grades from Infineon.