MOSFET (Si/SiC) Forum Discussions
Hi infineon
Could you know that AIMBG120R020M1 creepage distance shows high voltage only 800V? but VDS support 1200V
Any solution can confirm support to 1200V ?
Thanks
Hi Team,
Customer had IMW120R060M1H to replace wolfspeed C2M0080120D.
Customer have questions below question would like to clarify.
- From the graph below, the gate resistor is 100ohm. The negative current is around -0.8A. However, the MOSFET is very hot. They have tested with 10ohm gate resistor, but the negative current up to -2.3A observed. Will negative current spike of 2.3A cause any reliability issue to the SIC MOSFET?
- What is the max negative current the SIC MOSFET can sustain?
- If the negative current will cause reliability issue, how to improve the ringing?
The brightness below refers to the load level. 100% Brightness = full load, 10% Brightness =light load
Customer is using flyback controller to drive the SIC MOSFET.
MOSFET Waveform (Ch1=Vds, Ch2=Vgs, Ch4=Ids)
Fig.1 : 100% Brightness
Fig.2 : 40% Brightness
Fig.3 : 30% Brightness
Fig.1 : 20% Brightness
Fig.4 : 10% Brightness
Schematic (Output 350W 500V 700mA)
Show Less
Hello IFXer,
Since trench gate SIC MOSFET has narrow nagative voltage window compare with planner gate SIC MOSFET.
we are care about the gate driver whether build in miller clamp and use zero voltage to turn off SIC MOSFET.
but there is all half bridge topology need use miller clamp function? please help advise.
hard switch: buck, boost, totem pole
soft switch: ACF flyback, LLC, phase shift full bridge
Hi,
Need your support to download spice and LT spice simulation models for IPT030N12N3 G .
Thanks
Ravi
Dear Infineon team,
I have an issue with using Infineon Spice model in LTspice as shown in attached picture. I think it is about the setting up of Tj and T1 terminals for junction temperature and case temperature.
The device I use is IPWS65R022CFD7A.
Could you please help me to solve this issue?
Many thanks.
Alex
Show Less
What is the ‘Maximum Pulsed Source to Drain Diode Forward Current’ for the part IPA65R150CFDXKSA1?
I think there is a loss due to Coss(esr) when zvs.
Is there a way to find the loss?
Hello,
We are using the Power MOSFET IPB083N15N5LF in our power supply product.
I have a question on the safe operating temperature range measured on the package top face.
In our product the bottom tab is mounted on the heatsink.
When I measure the temperature at the package top face by using a thermocouple under the rated load, it is measured as 73℃ for the environmental temperature of 27℃.
Therefore we suppose that the temperature at the package top face under the rated load would be 96℃ and 117℃ for the environmental temperature of 50℃ and 71℃ respectively.
I wonder how much the Power MOSFET IPB083N15N5LF is safe when the temperature at the package top face is measured as 96℃ and 117℃ respectively.
Thank you for your guidance.
With regards,
GKIM
Show LessHello IFXer,
How to quantify the tpulse,positive<=1%dutycycle/fsw test condition for Vgs transient?
we compare other trench gate vendor, just show simple test condition such as tsurge < 300ns.
Show Less