Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

MOSFET (Si/SiC) Forum Discussions

MOSFET (Si/SiC) Forum Discussions

Sort by:
PowerStarter_
MOSFET (Si/SiC)
Hello, is there any source, where a table can be found, which contains the switching-frequency of the following Transistors? GaN, SiC, Si, IGBT, ... I... Show More
Sachin_alu
MOSFET (Si/SiC)
Hello infineon support  Am looking for basic understanding on how to calculate the mosfet gate resistance. I found the design link here but it doesn't... Show More
KUOWENYUNG
MOSFET (Si/SiC)
Hi IFXer, SI/SIC MOSFETs all generate parasitic diodes through internal P+ - N- - N+ (PiN),But why the reason for the lower Qrr of SIC MOSFET ? Is it ... Show More
xiaochuang
MOSFET (Si/SiC)
  When the MOS transistor spw55n80c3 was opened, the rising speed of the driving waveform was slow. It took 400ns to stay at Maitreya platfo... Show More
KUOWENYUNG
MOSFET (Si/SiC)
Dear Sir, How to evaluate power device junction temperature, at the time of Eon?For example, the power dissipation I see is about 6kW+2.3kW,Is my temp... Show More
MaKo_4831421
MOSFET (Si/SiC)

IPL60R360P6S
IPLK60R360PFD7

同じThinPAK 5 x 6の上記2製品のPackage形状が異なる。
そのままピンコンパチで載せ替え可能か。
また、フットプリントなどの詳細情報が欲しい。

TaOn_4865801
MOSFET (Si/SiC)

BSZ22DN20NS3 (S3O8)の実装後の推奨リワーク方法を教えてください
参考となる資料はありますか?

Ankit_singh
MOSFET (Si/SiC)
  I was using n channel power mosfet  AUIRFP4110.   by applying Vgs=12 V (in series  with 1k resistor) , Parallel resistance between GS was 1K(for fa... Show More
CL929
MOSFET (Si/SiC)
Hello there, Good Day. Would like to seek your help to confirm if it is normal to have the physical shape of IRLR9343TRPBF (DPAK) different from the d... Show More
MS_19060803
MOSFET (Si/SiC)
いつもお世話になっております。 IPA80R1K4P7を検討しております。基板の制約上、シャーシ(アース)との距離が近くなりそうなため IPA80R1K4P7のケース表面から内部素子導電部までの絶縁耐圧が分かりましたらご教示頂けませんでしょうか? 以上、よろしくお願いいたします。 Show More
Forum Information

MOSFET (Si/SiC)

Power MOSFETs have become an integral part of most of industrial and automotive applications, and Infineon offers leading-edge solutions to suit all needs. Infineon’s innovative OptiMOS™, CoolMOS™, and StrongIRFET™ low and medium voltage power MOSFETs consistently meet the highest quality and performance demands in key specifications for power system design, such as on-state resistance and figure of merit characteristics. Additionally, CoolMOS™ superjunction MOSFET offers a whole host of options for consumer, industrial, and automotive applications such as lighting, TV, audio, server/telecom, solar, EV charging, DC-DC converter, onboard chargers, and many more . In this forum, you can post your questions, comments, and feedback about Si/ SiC MOSFET of both industrial and automotive grades from Infineon.