MOSFET (Si/SiC) Forum Discussions
Hi,
I am performing the radiation analysis of a product implementing the IRHG567110 and would nee to know its sensitive depth in order to be able to assess its sensitvity to SEGR/SEB. Could you please provide me this confirmation?
Thanks and best regards
Fred
Show LessWhere is the safe operating area for continuous current?
Can this device handle 21 V @ 10 A continuous without a heatsink?
https://www.infineon.com/dgdl/irf8714pbf.pdf
Show LessWe've been using the FF3MR12KM1 power modules for a design. It appears they are discontinued. Is there an updated/newer version that's both mechanically a drop in replacement as well as an electrical drop in with minimum or acceptable differences?
Show LessIf everything remains the same after the IRF5210 is on the machine, other than the short circuit caused by excessive current, there will be no response to the short circuit phenomenon
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/MOSFET-Si-SiC/IRF5210-%E4%B8%8A%E6%9C%BA%E5%90%8E%E5%9C%A8%E4%B8%80%E5%88%87%E9%83%BD%E6%AD%A3%E5%B8%B8%E7%9A%84%E6%83%85%E5%86%B5%E4%B8%8B%E7%AA%81%E7%84%B6%E7%9F%AD%E8%B7%AF-%E6%98%AF%E4%B8%8D%E6%98%AF%E7%89%A9%E6%96%99%E6%9C%AC%E8%BA%AB%E8%B4%A8%E9%87%8F%E9%97%AE%E9%A2%98/td-p/649126
Show LessIs there a LTSpice simulation model for P-Ch(SuperSO8 5×6) FET?
I can't find it on the web page and would like to have a LTspice model of the following 4 product names.
The one I received before was a model for PSpice.
Solved: Re: About the P-Channel MOSFET (SuperSO8 5×6) Spic... - Infineon Developer Community
Show LessHello,
Using LTSpice (x64) Version 17.1.15
I've downloaded the OptiMos Library following: Infineon-OptiMOS_PowerMOSFET_PSpice_80V_N-Channel-SimulationModels-v03_00-EN and using the following library: StrongIRFET_80V_LTSpice.lib
When adding the following part to a simulation: IPB016N08NF2S_L1
I receive the following error: 'Undefined subcircuit: S5_80_f2_var'
...I have referenced the 'How to fix common errors in LTspice model simulation' here in the forum and it suggests the following: "To run the same model in LTspice, contact technical support team for the modified version of the file."
I've submitted a request to Technical support, yet I thought I'd post here as well to see if anyone can confirm if I am missing something...
Thank you in advance,
Iain
Show Less
Hello! Hello! Do you have the recommended reflow profile for the IRHN9150?
Thank you!
I purchased this IRF5803D2TRPBF. Can you tell if it is a 1039+or 2039+through screen printing?
Does Infineon have any Theta JB data for the SMD-0.5 package, or perhaps specifically JANSR2N7660U3CE and JANSR2N7648U3?
Many cool SIC MOSFET models, such as infineon-coolsic_silicon_carbide_mosfeet_1200v_spice-simulationmodels-v01_03-en, will report syntax errors when imported into Saber.
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/MOSFET-Si-SiC/spice%E6%A8%A1%E5%9E%8B%E5%AF%BC%E5%85%A5saber%E6%8A%A5%E8%AF%AD%E6%B3%95%E9%94%99%E8%AF%AF/td-p/648045
Show Less