Using infineon models in Orcad

Announcements

Live Webinar: Solving the challenges in xEV power conversions | March 7 @9am & 5pm CET. Register now!

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
lock attach
Attachments are accessible only for community members.
Not applicable
Hello,

I am trying use the simulation models of the ir2010 driver and irfb4321 mosfet in OrCAD. Both devices show the same problem during simulation:
ERROR -- Convergence problem in transient analysis at Time = 40.01E-15
Time step = 9.766E-18, minimum allowable step size = 10.00E-18

These devices failed to converge:
X_U2.D2

In the case of the ir2010 there is an OrCAD simulation model provided while with the irfb4321 the model is .spi and I save it as .lib with de MODELED program
I attach the caputure file folders (35.zip is ir2010 and 34.zip irbfb321)
0 Likes
1 Solution
User270
Level 5
Level 5
5 solutions authored First solution authored
See section 6.2 For ORCAD and change the settings for the simulation options.
LINK

View solution in original post

0 Likes
1 Reply
User270
Level 5
Level 5
5 solutions authored First solution authored
See section 6.2 For ORCAD and change the settings for the simulation options.
LINK
0 Likes