Announcements

Live Webinar: Solving the challenges in xEV power conversions | March 7 @9am & 5pm CET. Register now!

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
lock attach
Attachments are accessible only for community members.
Farco
Level 1
Level 1
First like received First reply posted First like given

Hello, I have a question abouot the Junciton-to-ambient thermal resistance of IRLR2908PbF MOSFET:

The datasheet specifies 40 °C/W referring to a note at the end of the document:
Farco_0-1655243355229.png

The note states that this value is valid "When mounted on 1" square PCB (FR-4 or G-10 Material)." It also says: "For recommended footprint and soldering techniques refer to application note #AN-994"

Here is my question: Is the note referring to a 1 in^2 copper pad below the device (as AN-994 recommends) or is it only the area of the PCB with the device mounted in a minimum footprint?

Best Regards.

0 Likes
1 Solution
lock attach
Attachments are accessible only for community members.
sushank
Moderator
Moderator
Moderator
25 solutions authored 100 sign-ins 50 replies posted

Hi there,

this is the area of the PCB, and the Mosfet will be sitting inside this area on the footprint that is cu pad. 

you can also check the mosfet maximum area, that is E*H = 0.265*0.410 = 0.10865 inch^2 which is less than 1 inch^2.

Thanks. 

 

View solution in original post

2 Replies
lock attach
Attachments are accessible only for community members.
sushank
Moderator
Moderator
Moderator
25 solutions authored 100 sign-ins 50 replies posted

Hi there,

this is the area of the PCB, and the Mosfet will be sitting inside this area on the footprint that is cu pad. 

you can also check the mosfet maximum area, that is E*H = 0.265*0.410 = 0.10865 inch^2 which is less than 1 inch^2.

Thanks. 

 

Farco
Level 1
Level 1
First like received First reply posted First like given

Alright, thank you for the support!