- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I brought the PSPICE model into LTSPICE and added external stray inductances of 6.8 nH to the leads and found that there was up to 35 volts of overshoot at the gate even with 10 Ohm external gate resistor.
I know that the overshoot is caused by resonance from the inductance and the effective gate capacitance of which CGDO contributes and that critical damping occurs when the gate resistor = 1/2 x sqrt (L_stray/C). So a low value of capacitance would result in an underdamped response with ringing.
I then looked at the model and found that the CGDO value was only 10 pF. I looked at a similar Power MOSFET and it had much higher CGDO, about 68 nF. I then removed the IRHYS9A7234CM model from my schematic and substituted the other MOSFET model. I saw no ringing or overshoot with the other model.
My question is : is the CGDO value correct in the irhys9a7234cm model?
I pasted the SPICE model for the IRHYS9A7234CM (that exhibits the overshoot) below.
Regards,
Ken
.SUBCKT irhys9a7234cm 1 2 3
**************************************
* Model Generated by MODPEX *
*Copyright(c) Symmetry Design Systems*
* All Rights Reserved *
* UNPUBLISHED LICENSED SOFTWARE *
* Contains Proprietary Information *
* Which is The Property of *
* SYMMETRY OR ITS LICENSORS *
*Commercial Use or Resale Restricted *
* by Symmetry License Agreement *
**************************************
* Model generated on Nov 7, 19
* MODEL FORMAT: SPICE3
* Symmetry POWER MOS Model (Version 1.0)
* External Node Designations
* Node 1 -> Drain
* Node 2 -> Gate
* Node 3 -> Source
M1 9 7 8 8 MM L=100u W=100u
.MODEL MM NMOS LEVEL=1 IS=1e-32
+VTO=3.90376 LAMBDA=0.129709 KP=33.9959
+CGSO=1.60177e-05 CGDO=1e-11
RS 8 3 0.0804021
D1 3 1 MD
.MODEL MD D IS=9.9526e-09 RS=0.011175 N=1.5 BV=250
+IBV=0.001 EG=1 XTI=3.09708 TT=1e-07
+CJO=1.10724e-08 VJ=0.5 M=0.9 FC=0.5
RDS 3 1 5e+07
RD 9 1 0.0001
RG 2 7 21.1069
D2 4 5 MD1
* Default values used in MD1:
* RS=0 EG=1.11 XTI=3.0 TT=0
* BV=infinite IBV=1mA
.MODEL MD1 D IS=1e-32 N=50
+CJO=3.56975e-11 VJ=0.5 M=0.9 FC=1e-08
D3 0 5 MD2
* Default values used in MD2:
* EG=1.11 XTI=3.0 TT=0 CJO=0
* BV=infinite IBV=1mA
.MODEL MD2 D IS=1e-10 N=0.4 RS=3e-06
RL 5 10 1
FI2 7 9 VFI2 -1
VFI2 4 0 0
EV16 10 0 9 7 1
CAP 11 10 1.17096e-09
FI1 7 9 VFI1 -1
VFI1 11 6 0
RCAP 6 10 1
D4 0 6 MD3
* Default values used in MD3:
* EG=1.11 XTI=3.0 TT=0 CJO=0
* RS=0 BV=infinite IBV=1mA
.MODEL MD3 D IS=1e-10 N=0.4
.ENDS irhys9a7234cm
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
Thank you for sharing the model. I realized in the datasheet it is mentioned Ls+Ld,the total inductance value equals 6.8nH, not individually. We cannot take the lead inductance value as 6.8nH it should be lower than that(for Ls and Ld). Putting any value greater than 6.8nH will worsen the situation and result in an overshoot.
Regards,
Anshika
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello Ken,
Thankyou for posting on Infineon Community.
The Infineon spice models have verified models and should result accurately with the specifications provided in the model.
I infer that you want to make your circuit operate at resonant conditions and that is why you are adding external inductance to it. Please let me know if there is something more to it.
Can you please check without the external inductance or with a small value of it and share the results?
If you stimulate the resonant circuit with a fast positive or negative edge, it will resonate, which includes overshoot and undershoot. I understand that when you have tried with a high capacitance value , the gate resistor value will be small and it results in no overshoot.
Regards,
Anshika
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I attached a set of slides showing the gate voltage overshoot with 0.001 nH (basically no inductance) in series with each of the three MOSFET leads vs 6.8 nH in series with each of the MOSFET leads (which is the datasheet lead inductance) on all three leads.
In both cases the gate resistance is 2 Ohms and is modeled as an external resistor on the simulation schematic between the MOSFET driver and the MOSFET gate lead.
There is an unexpected overshoot at the gate that pushes the gate voltage above the 20 volt absolute maximum.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
Thank you for sharing the results.
From the graphs shared by you, it is clear that Cgdo value alone does not cause any issue if used without inductance, but overshoots when do.
I am hoping that you have considered both the capacitances Cgso and Cgdo in your simulation model. If not, please do as Cgso has great significance while doing simulation or real-time modelling.
Cgso and Cgdo are overlap capacitance that occur because of some manufacture imperfections or so, they are not junction capacitances as Cgs and Cgd. In the datasheet, the value of input capacitance Ciss is given, can you please use this value and test your circuit:
If possible, please share your circuit so that I can also test it and answer you in a better way.
Regards,
Anshika
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I don't see Ciss in the SPICE model I am using (pasted here). Am I missing it?
I know that Ciss is a combination of Cgs and Cgd and that Cgd changes with VDS voltage (because of the Miller Effect), so I'm just wondering how to accurately model Ciss (without, for instance, an if-then statement to account for the various values of Cgd during the various stages of turn-on).
I'll work on getting you a simulation file that you can run. I may have to get approval to send it to you.
Ken
.SUBCKT irhys9a7234cm 1 2 3
**************************************
* Model Generated by MODPEX *
*Copyright(c) Symmetry Design Systems*
* All Rights Reserved *
* UNPUBLISHED LICENSED SOFTWARE *
* Contains Proprietary Information *
* Which is The Property of *
* SYMMETRY OR ITS LICENSORS *
*Commercial Use or Resale Restricted *
* by Symmetry License Agreement *
**************************************
* Model generated on Nov 7, 19
* MODEL FORMAT: SPICE3
* Symmetry POWER MOS Model (Version 1.0)
* External Node Designations
* Node 1 -> Drain
* Node 2 -> Gate
* Node 3 -> Source
M1 9 7 8 8 MM L=100u W=100u
.MODEL MM NMOS LEVEL=1 IS=1e-32
+VTO=3.90376 LAMBDA=0.129709 KP=33.9959
+CGSO=1.60177e-05 CGDO=1e-11
RS 8 3 0.0804021
D1 3 1 MD
.MODEL MD D IS=9.9526e-09 RS=0.011175 N=1.5 BV=250
+IBV=0.001 EG=1 XTI=3.09708 TT=1e-07
+CJO=1.10724e-08 VJ=0.5 M=0.9 FC=0.5
RDS 3 1 5e+07
RD 9 1 0.0001
RG 2 7 21.1069
D2 4 5 MD1
* Default values used in MD1:
* RS=0 EG=1.11 XTI=3.0 TT=0
* BV=infinite IBV=1mA
.MODEL MD1 D IS=1e-32 N=50
+CJO=3.56975e-11 VJ=0.5 M=0.9 FC=1e-08
D3 0 5 MD2
* Default values used in MD2:
* EG=1.11 XTI=3.0 TT=0 CJO=0
* BV=infinite IBV=1mA
.MODEL MD2 D IS=1e-10 N=0.4 RS=3e-06
RL 5 10 1
FI2 7 9 VFI2 -1
VFI2 4 0 0
EV16 10 0 9 7 1
CAP 11 10 1.17096e-09
FI1 7 9 VFI1 -1
VFI1 11 6 0
RCAP 6 10 1
D4 0 6 MD3
* Default values used in MD3:
* EG=1.11 XTI=3.0 TT=0 CJO=0
* RS=0 BV=infinite IBV=1mA
.MODEL MD3 D IS=1e-10 N=0.4
.ENDS irhys9a7234cm
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Ken,
Yes,you are correct,the Ciss is not mentioned in the SPICE model and it would be difficult to analyze the behavior accurately. Have you checked for Cgso value also for the irhys9a7234cm and the other Mosfet that you have used?
I would appreciate if you can share the model.
Regards,
Anshika
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi ,
Here is a plot of the gate voltage. I attached the zipped LTSPICE file. Note that the gate resistor and board inductance associated with the MOSFET pins are parameters that can be changed and right now the gate resistor is fairly large value at 11 Ohms and the stray inductance is 19.7 nH which is a value consistent with 2 inches of AWG18 wire.
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
Hello,
Thank you for sharing the model. I realized in the datasheet it is mentioned Ls+Ld,the total inductance value equals 6.8nH, not individually. We cannot take the lead inductance value as 6.8nH it should be lower than that(for Ls and Ld). Putting any value greater than 6.8nH will worsen the situation and result in an overshoot.
Regards,
Anshika
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Where to Buy CSGO Prime Accounts?.
Buy CSGO Prime Account online for an affordable price and start your quality CSGO career. This gives you an excellent possibility of moving ahead in the game. You can select accounts that are at different ranks, that have miscellaneous kinds of skin, those with the most success ratio, and substantially more. It is very much like glancing for your patronage CSGO Service Medal account.
You can get the new accounts as per your choice, and once you finalize the account, you will be encouraged to make the payment by sending the account details to your email id. It is 100% safe and secure. Once you make the payment, your gaming career will start in Counter-Strike, and you will reach a new higher level.
Firstly, A Prime ranked Account of CSGO is one that has already completed hours of play. It is the one that has covered so much activity and surpassed a long winning streak. Secondly, all you need to do is buy the account from our marketplace and start gaming.
The conclusion is that buying a csgo ranked account will save a lot of time and lots of energy. You will also get the higher rank teammates who are like experienced players, and playing along with them makes the day perfect. So, For this, you need to spend a few dollars and grab a CSGO that will help you cross all those hackers and cheaters and help you play the game with a lot of enjoyment & Fair.
https://www.buyprimeaccount.com
https://www.csgoprimeaccount.com