Announcements

Live Webinar: Solving the challenges in xEV power conversions | March 7 @9am & 5pm CET. Register now!

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Not applicable
What is repetitive avalanche energy and repetitive avalanche current for CoolMOS?
0 Likes
1 Solution
yifei_y
Moderator
Moderator
Moderator
25 likes received 100 solutions authored 100 sign-ins
Repetitive avalanche energy is the maximum permissible reverse-voltage breakdown energy in continuous operation while observing the maximum permissible chip temperature. Repetitive avalanche operation refers to repeated single shot-avalanche events and involves additional parameters such as frequency of the application. IAR, repetitive avalanche current is the maximum allowed peak load current passing through the MOSFET before turn-off at repetitive reverse-voltage breakdown loading. Exceeding IAR (even without exceeding EAR) can lead to destruction of the device due to current oscillations within the MOSFET. IAS (single pulse avalanche current) is not specified in the datasheet because both IAS and IAR are both limited by current oscillations and not by thermal limitation of the device. Hence, the maximum avalanche current is always the same, no matter if in single shot or repetitive operation.

View solution in original post

0 Likes
1 Reply
yifei_y
Moderator
Moderator
Moderator
25 likes received 100 solutions authored 100 sign-ins
Repetitive avalanche energy is the maximum permissible reverse-voltage breakdown energy in continuous operation while observing the maximum permissible chip temperature. Repetitive avalanche operation refers to repeated single shot-avalanche events and involves additional parameters such as frequency of the application. IAR, repetitive avalanche current is the maximum allowed peak load current passing through the MOSFET before turn-off at repetitive reverse-voltage breakdown loading. Exceeding IAR (even without exceeding EAR) can lead to destruction of the device due to current oscillations within the MOSFET. IAS (single pulse avalanche current) is not specified in the datasheet because both IAS and IAR are both limited by current oscillations and not by thermal limitation of the device. Hence, the maximum avalanche current is always the same, no matter if in single shot or repetitive operation.
0 Likes