Need Mosfet Voltage/current calculation for single H- Bridge to drive Motor

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
kumarluc
Level 3
Level 3
Distributor - NEXTY (India)
10 questions asked First solution authored 5 replies posted

Hi

I am working on 400W/12V motor control by using single Phase H-Bridge & need calculation data for mosfet.

Regards

Lucky Kumar

 

0 Likes
1 Solution
vigneshkumar
Moderator
Moderator
Moderator
25 likes received 250 sign-ins 50 solutions authored

MOSFET Selection:

Breakdown voltage

BVDSS – 1.3 times the Max Vds applied, if the it is connected to a Battery then the BVDSS should be equal to  VBAT  for the full bridge and 2VBAT­ for half bridge

Drain current Id

 For a easy selection you can check the Id@Tc 100Deg C  in datasheet should be more than the Id-Max Applied.

If you want to optimise for the particular case temperature

vigneshkumar_0-1704215827263.pngvigneshkumar_1-1704215827264.png

Id@Tc should be more than max Id applied.

 

Qg,Qrr, avalanche energy, short circuit ruggedness is need to be checked. For more info please refer the below link

https://www.infineon.com/dgdl/Infineon-MOSFET_selection_for_low_voltage_UPS-ApplicationNotes-v01_01-...

file:///C:/Users/ShanmugamVig/Downloads/Infineon-WhitePaper_PowerLoss_and_Optimized_MOSFET_Selection...

Regards

Vignesh

View solution in original post

0 Likes
1 Reply
vigneshkumar
Moderator
Moderator
Moderator
25 likes received 250 sign-ins 50 solutions authored

MOSFET Selection:

Breakdown voltage

BVDSS – 1.3 times the Max Vds applied, if the it is connected to a Battery then the BVDSS should be equal to  VBAT  for the full bridge and 2VBAT­ for half bridge

Drain current Id

 For a easy selection you can check the Id@Tc 100Deg C  in datasheet should be more than the Id-Max Applied.

If you want to optimise for the particular case temperature

vigneshkumar_0-1704215827263.pngvigneshkumar_1-1704215827264.png

Id@Tc should be more than max Id applied.

 

Qg,Qrr, avalanche energy, short circuit ruggedness is need to be checked. For more info please refer the below link

https://www.infineon.com/dgdl/Infineon-MOSFET_selection_for_low_voltage_UPS-ApplicationNotes-v01_01-...

file:///C:/Users/ShanmugamVig/Downloads/Infineon-WhitePaper_PowerLoss_and_Optimized_MOSFET_Selection...

Regards

Vignesh

0 Likes