MOSFET - Datasheet help

Announcements

Live Webinar: Solving the challenges in xEV power conversions | March 7 @9am & 5pm CET. Register now!

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
User20208
Level 1
Level 1
First question asked
Hi,

A N-Channel Mosfet when in the on-state and no drain/load current flowing, the Vds voltage would be zero (i.e differential voltage across drain and source). At this point, when a load connected to mosfet's source is switched on by an external switch would draw a 50A of DC current. How to interpret the SOA curve
at these conditions when drain/load current begins to flow and Vds (voltage Vds = 0V, i.e 48V on either side as an example)

Example mosfet: https://www.infineon.com/dgdl/Infineon-IPB017N10N5-DataSheet-v02_05-EN.pdf?fileId=5546d4624a75e5f101...

Can any one help me explaining how to interpret the SOA curve?

Thanks for the help.
0 Likes
1 Solution
Anshika_G
Moderator
Moderator
Moderator
50 likes received 250 replies posted 100 solutions authored

Hello,

Thank you for posting on Infineon Community.

The safe operating area is the voltage and current conditions over which a MOSFET operates without permanent damage or degradation. The MOSFET must not be exposed to conditions outside the safe operating area, even for an instant. Therefore, it is necessary to determine whether the operating locus of the MOSFET is within the safe operating area.
There are five limit-lines defining the SOA diagram are the RDS(on) limit-line (blue line), the current limit-line (red line), the maximum power limit-line(dark green line), the thermal instability limit-line (light green line) and the breakdown voltage limit-line (yellow line).

G_Anshika_0-1643903087862.png

Within these limit-lines the green shaded area gives the area where the MOSFET can be safely operated.


1. RDS(on)-limit-line (blue line)
2. Package-limit-line (red line)
3.Maximum-power-limit-line
4. Thermal (in-)stability limit-line
5. Breakdown voltage limit-line

Please refer to this Application Note for more details:
Infineon-ApplicationNote_Linear_Mode_Operation_Safe_Operation_Diagram_MOSFETs-AN 
I hope this helps. 

Thanks and Regards,
Anshika
                                

View solution in original post

0 Likes
2 Replies
User270
Level 5
Level 5
5 solutions authored First solution authored
Please see page 9 in the following app note.
0 Likes
Anshika_G
Moderator
Moderator
Moderator
50 likes received 250 replies posted 100 solutions authored

Hello,

Thank you for posting on Infineon Community.

The safe operating area is the voltage and current conditions over which a MOSFET operates without permanent damage or degradation. The MOSFET must not be exposed to conditions outside the safe operating area, even for an instant. Therefore, it is necessary to determine whether the operating locus of the MOSFET is within the safe operating area.
There are five limit-lines defining the SOA diagram are the RDS(on) limit-line (blue line), the current limit-line (red line), the maximum power limit-line(dark green line), the thermal instability limit-line (light green line) and the breakdown voltage limit-line (yellow line).

G_Anshika_0-1643903087862.png

Within these limit-lines the green shaded area gives the area where the MOSFET can be safely operated.


1. RDS(on)-limit-line (blue line)
2. Package-limit-line (red line)
3.Maximum-power-limit-line
4. Thermal (in-)stability limit-line
5. Breakdown voltage limit-line

Please refer to this Application Note for more details:
Infineon-ApplicationNote_Linear_Mode_Operation_Safe_Operation_Diagram_MOSFETs-AN 
I hope this helps. 

Thanks and Regards,
Anshika
                                

0 Likes