Announcements

Join us for FREE at OktoberTech Asia Pacific and hear about decarbonizing future mobility. Click here for more details.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

MOSFET (Si/SiC) Forum Discussions

Not applicable
How can IR25750 be used to sense the current in a low-side and a high side MOSFET?
0 Likes
1 Solution
Not applicable
The IR25750 current sensing IC can measure the VDS (on) of a MOSFET or the VCE (on) of an IGBT. *You can read more about how to set up such an application circuit targeting either type of device in AN-1199.

The IR25750 targets only low-side MOSFET configurations.*The device could theoretically target a high-side MOSFET. *However, keep in mind that the output would then be a reference to the VS node which is a floating high voltage that would make the output unusable to anything referenced to GND as it would be a very high voltage because the output signal (CS) is referenced to the COM pin of the IC.

View solution in original post

0 Likes
1 Reply
Not applicable
The IR25750 current sensing IC can measure the VDS (on) of a MOSFET or the VCE (on) of an IGBT. *You can read more about how to set up such an application circuit targeting either type of device in AN-1199.

The IR25750 targets only low-side MOSFET configurations.*The device could theoretically target a high-side MOSFET. *However, keep in mind that the output would then be a reference to the VS node which is a floating high voltage that would make the output unusable to anything referenced to GND as it would be a very high voltage because the output signal (CS) is referenced to the COM pin of the IC.
0 Likes