I can not Filtering mosfet with minimum Qg

Announcements

Live Webinar: Solving the challenges in xEV power conversions | March 7 @9am & 5pm CET. Register now!

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
User17008
Level 1
Level 1
First question asked First reply posted
Hello, I want mosfets N with

RDS (on) @10V max 8 mohm
VBRDSS >= 30
VGS(th) max 2.2 V
ID @ TC=25°C min 59 A
QG typ @10V < 12 nC

I go to
https://www.infineon.com/cms/en/product/power/mosfet/20v-300v-n-channel-power-mosfet/

and put the filters
RDS (on) @10V max 0.4 - 8
VGS(th) max 0.5 - 2.2
ID @ TC=25°C max 59 - 462

https://www.infineon.com/cms/en/product/power/mosfet/20v-300v-n-channel-power-mosfet/?filterValues=~...

The QG filter not work ! I can not to put my value

and I get only 2 mosfet !

I can not believe that there are only 2 mosfet with this filter but
some mosfets not have parameters in the table or the filter not working fine or
I not know how to use the filter page

How I can find more power mosfets inside infineon with this parameters ?

And If this posible with package
TO-220,TO-220 Full Pack,TO-247,TO-251,TO-251 SL 251-3 251-3-11
TO-252-3-23,TO-262,TO-263-3L,TO-273,TO-274,Super-220,Super-247,I2Pak

Thank you
in advance
0 Likes
1 Solution
2 Replies
lifesaprototype
Employee
Employee
First comment on blog 10 sign-ins 5 sign-ins
0 Likes
User17008
Level 1
Level 1
First question asked First reply posted
ok, If I go to
https://www.infineon.com/cms/en/tools/solution-finder/product-finder/mosfet-finder/
and put
Breakdown Voltage 30
and
Drain Current ID(max) at least 50
I view 61 Results

why, for example, the IRLB8314PbF does not appear ?

Tks
0 Likes