Announcements

Live Webinar: Solving the challenges in xEV power conversions | March 7 @9am & 5pm CET. Register now!
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
How many MOSFETS (IRFS4115) can Driver IRS21864S drive?

0 Likes
1 Solution
Translation_Bot
Community Manager
Community Manager
Community Manager

Hello @wanglipeng00000,

This really depends on the specific application conditions, such as switching frequency, operating temperature, etc

View solution in original post

0 Likes
3 Replies
Translation_Bot
Community Manager
Community Manager
Community Manager

Hello @wanglipeng00000,

This really depends on the specific application conditions, such as switching frequency, operating temperature, etc

0 Likes
Translation_Bot
Community Manager
Community Manager
Community Manager

Hi,   , thanks  very much, but If the   switching frequency is 10KHZ,temperature is at beside in the range 0~50°,How many Mosfets(IR4115) can driver(IRS21864) drive? I now use this driver drive Max 16 mosfets, is that correct? 

0 Likes
Translation_Bot
Community Manager
Community Manager
Community Manager

Hello @wanglipeng00000!

You can make a rough calculation according to the driving current of the IRS21864S and the Qg of the...IRFS4115, Qg=I*tr, and then estimate an acceptable tr time according to the switching frequency of 10kHz and the switching cycle of 100us, and then add some margin according to the actual situation, so that you can roughly get a value.

0 Likes