Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
User21259
Level 1
Level 1
First question asked First reply posted
Hi everyone,

I'm working on a 350V / 40A converter application and i intend to use the F4-23MR12W1M1P_B11 Infineon power module.

To protect my converter in a short-circuit case, i'm using a current sensor with 500 ns delay and i added a 6.6 uH inductor to slow the current rise, but i found that the inductor is taking too much place in the converter and there is no place left for other components, so i need to remove it. My question is :
In a short-circuit case, what is the maximal current i'm gonna get ? can the power module handle it ? if yes, for how much time ?

Thank you
0 Likes
1 Reply
Abhilash_P
Moderator
Moderator
Moderator
50 likes received 500 replies posted 250 solutions authored
Hi,

Can you please provide the circuit details for analyzing it and calculating the exact short circuit current.
Also please provide the switching frequency and voltage levels.

Regards,
Abhilash P
0 Likes