Difference between SMD pad and NSMD Pad

Announcements

Live Webinar: Solving the challenges in xEV power conversions | March 7 @9am & 5pm CET. Register now!

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Not applicable
What is the difference between SMD pad and NSMD Pad?

And can you also give me a definition of these two?

Thanks!
0 Likes
1 Solution
Not applicable
“Solder mask defined” (SMD) pad : The copper metal pad is larger than the solder mask opening above this pad. Thus the pad area is defined by the opening in the solder mask.
Non-Solder Mask Defined” (NSMD) pad: Around each copper metal pad there is solder mask clearance. Dimensions and tolerances of the solder mask clearance have to be specified to ensure that the solder pad is not overlapped by the solder mask.
Depending on the PCB manufacturer’s tolerances, 75 µm is a widely used value

View solution in original post

0 Likes
1 Reply
Not applicable
“Solder mask defined” (SMD) pad : The copper metal pad is larger than the solder mask opening above this pad. Thus the pad area is defined by the opening in the solder mask.
Non-Solder Mask Defined” (NSMD) pad: Around each copper metal pad there is solder mask clearance. Dimensions and tolerances of the solder mask clearance have to be specified to ensure that the solder pad is not overlapped by the solder mask.
Depending on the PCB manufacturer’s tolerances, 75 µm is a widely used value
0 Likes