Level 2
NXTY_Fujioka
Level 2
Jun 07, 2021
01:23 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Could you let me the difference between CoolMOS CFD7 and PFD7?
I compared the IPA60R125CFD7 and IPAN60R125PFD7S, which have the same package and specs.
According to the datasheet, the IPA60R125CFD7 has ID(max)=11A, but the IPAN60R125PFD7S has ID(max)=25A.
What is the reason for this difference in specifications?
The rest of the specifications are almost the same, so I suspect that the chips inside are the same.
Are the chips in these the same?
If the chip inside is the same, the maximum value of ID should be the same, but why is it different?
Best regards,
Yuki
I compared the IPA60R125CFD7 and IPAN60R125PFD7S, which have the same package and specs.
According to the datasheet, the IPA60R125CFD7 has ID(max)=11A, but the IPAN60R125PFD7S has ID(max)=25A.
What is the reason for this difference in specifications?
The rest of the specifications are almost the same, so I suspect that the chips inside are the same.
Are the chips in these the same?
If the chip inside is the same, the maximum value of ID should be the same, but why is it different?
Best regards,
Yuki
Solved! Go to Solution.
1 Solution

Moderator

Moderator
Jun 20, 2021
05:24 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Hello Yuki,
I apologize for the late response.
The reason for the difference in Id between PFD7 to CFD7 is the following:
In the footnote of the datasheet we can see the following:

In other words, the rated current is defined for a duty cycle =50%. This is typically applied to all consumer/standard applications to which the PFD7 is targeted. You can see the same also applied to the CoolMOS P7 family.
On the other hand, there is no limitation of duty cycle for CFD7 current rating., since this part is fitting to high-end industrial applications.
There is in no way no significant difference in bonding between the two technologies.
Therefore, the difference in Id is just a difference in test settings, namely duty cycle.
I hope this clears your question.
Best regards,
Pablo
I apologize for the late response.
The reason for the difference in Id between PFD7 to CFD7 is the following:
In the footnote of the datasheet we can see the following:
In other words, the rated current is defined for a duty cycle =50%. This is typically applied to all consumer/standard applications to which the PFD7 is targeted. You can see the same also applied to the CoolMOS P7 family.
On the other hand, there is no limitation of duty cycle for CFD7 current rating., since this part is fitting to high-end industrial applications.
There is in no way no significant difference in bonding between the two technologies.
Therefore, the difference in Id is just a difference in test settings, namely duty cycle.
I hope this clears your question.
Best regards,
Pablo
5 Replies

Moderator

Moderator
Jun 07, 2021
11:36 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Hello Yuki,
Thank you for posting on Infineon Forums.
We are working on your question and we will get back to you as soon as we have an answer.
Best regards,
Pablo
Thank you for posting on Infineon Forums.
We are working on your question and we will get back to you as soon as we have an answer.
Best regards,
Pablo

Moderator

Moderator
Jun 15, 2021
05:52 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Hello Yuki,
I apologize for making you wait.
We are still working on your question, however, it is taking more time than expected.
Please wait a little more while we work on it.
Best regards,
Pablo
I apologize for making you wait.
We are still working on your question, however, it is taking more time than expected.
Please wait a little more while we work on it.
Best regards,
Pablo

Moderator

Moderator
Jun 20, 2021
05:24 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Hello Yuki,
I apologize for the late response.
The reason for the difference in Id between PFD7 to CFD7 is the following:
In the footnote of the datasheet we can see the following:

In other words, the rated current is defined for a duty cycle =50%. This is typically applied to all consumer/standard applications to which the PFD7 is targeted. You can see the same also applied to the CoolMOS P7 family.
On the other hand, there is no limitation of duty cycle for CFD7 current rating., since this part is fitting to high-end industrial applications.
There is in no way no significant difference in bonding between the two technologies.
Therefore, the difference in Id is just a difference in test settings, namely duty cycle.
I hope this clears your question.
Best regards,
Pablo
I apologize for the late response.
The reason for the difference in Id between PFD7 to CFD7 is the following:
In the footnote of the datasheet we can see the following:
In other words, the rated current is defined for a duty cycle =50%. This is typically applied to all consumer/standard applications to which the PFD7 is targeted. You can see the same also applied to the CoolMOS P7 family.
On the other hand, there is no limitation of duty cycle for CFD7 current rating., since this part is fitting to high-end industrial applications.
There is in no way no significant difference in bonding between the two technologies.
Therefore, the difference in Id is just a difference in test settings, namely duty cycle.
I hope this clears your question.
Best regards,
Pablo
Level 2
NXTY_Fujioka
Level 2
Jun 21, 2021
02:27 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Dear Pablo
Thank you for your answer.
In other words, are the two companies exactly the same except for the imprinting, just with different test conditions for ID?
If so, what is the reason for the price difference between IPA60R125CFD7 and IPAN60R125PFD7S?
Best regards,
Yuki Fujioka
Thank you for your answer.
In other words, are the two companies exactly the same except for the imprinting, just with different test conditions for ID?
If so, what is the reason for the price difference between IPA60R125CFD7 and IPAN60R125PFD7S?
Best regards,
Yuki Fujioka

Moderator

Moderator
Jun 21, 2021
02:52 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Hello Fujioka san,
CFD7 and PFD7 are different technologies.
The chips are not the same.
The CFD7 technology allows it to have higher robustness.
The fact that most parameters are similar is because they have been designed like that, not because the chip is the same.
These parts are not the same chip.
Best regards,
Pablo
CFD7 and PFD7 are different technologies.
The chips are not the same.
The CFD7 technology allows it to have higher robustness.
The fact that most parameters are similar is because they have been designed like that, not because the chip is the same.
These parts are not the same chip.
Best regards,
Pablo