Announcements

Live Webinar: Solving the challenges in xEV power conversions | March 7 @9am & 5pm CET. Register now!

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
User17477
Level 1
Level 1
First question asked First reply posted
I have constructed an H-Bridge using two IR2101S driver ICs and four IRFZ44N power FETs, it works and there are no problems.

I have now been given an additional requirement of bias voltages on the bridge output so, for example, I now supply a square wave that varies between 1.8V and Vsupply to the load.
How can I do this? Should I supply a variable gate bias to two of the FETs (and risk destroying the driver ICs) or should I put bias resistors on the output and possibly alter the pulse shape?

The circuit used is the standard one from the data sheet and the gate resistors are 22 ohms. Vsupply is 25V

Regards

Peter Gant
Lab Technician
ACST GmbH
0 Likes
2 Replies
lifesaprototype
Employee
Employee
First comment on blog 10 sign-ins 5 sign-ins
Hi Peter,

so you need a positive square wave with a high level of 25V and a low level 1.8V?
Would PWM with a low duty cycle be a possible solution in the low level state?
0 Likes
User17477
Level 1
Level 1
First question asked First reply posted
Sorry, no, I do not think that PWM would work in this application. I cannot go too far into details but the requirement is for an H-Bridge to supply fast pulses to a load in either direction with (ideally) nice sharp edges on the pulses.
If I add a capacitor across the load so that I can do PWM this would destroy the pulse shape.

So, is it possible to bias an H-Bridge into linear operation or are the power FETs only designed for on-off operation?

Regards

Peter Gant
Lab Technician
ACST GmbH
0 Likes