Hi,
After long datasheets reading and many fail attempts I have launched these two boards combined together.
Here is what you have to do:
1. Load project from IRMCS0199-1-M1 folder with MCE Designer.
2. Program firmware IRMCK099FirmwareV15 to RAM from the same IRMCS0199-1-M1 folder.
3. Now open TinyWizard software, select IRMCS0199-1-M1 demo board, mark both check box options and start yours own configuration.
Some configuration will depend on yours motor, these you will have to find out, but some you can use from configuration file I have attached.
4. Export whole configuration to .txt file and load it to the MCE Designer.
5. Load configuration to the board by pressing "Configure Motor" button.
6. Try to start it...
You can also load config.txt file to the MCEWizard, just rename it config.tw
Regards,
Gintaras