Hello,
The IRMCK099 Series Reference Manual has a very nice section 3.5 Custom Programming Methods, describing in a fair level of detail what has to be done in order to program the part via JTAG with any other method, but the IR Cable. This is somewhow my scenario, as I need to program configure (via JTA) and control (via UART) the IRMCK099 from an external host MCU.
The reason is the obvious one: development and iterative testing. For that, programming the OTP is not the recommended method, but rather to download the Firmware and Parameters to RAM is what I need to do. But here, the documentation miserably fails: section 3.4 Download to RAM of IRMCK099 Series Reference Manual simply says "Kindly refer to IRCable V2 user manual for step by step process of downloading the firmware into RAM".
Where can I find information for downloading to RAM of the IRMCK099 by "Custom Method", not the IR Cable thing? I can not find the so called IRCable V2 user manual.
Kind regards.