Low Noise Amplifiers Forum Discussions
Hi,
I need a power amplifier that will be used in 4G LTE Band 65 (2100-2200 MHz). The power output needed is 1W.
The device will be used in a cubesat so high efficiency is also needed.
Is there any product that you can recommend me for such an application?
Thanks!
Show LessHi Infineon
We know the BGA525N6 absolute maximum ratings for temperature (-40~-85) , can you tell us the recommended operating temperature conditions, thank you !
Show Less
Hi,
I can't see the normal voltage specifications for the enable and bypass inputs on the BGA729N6? There are absolute maximum ratings to limit the applied voltage to between the supply and ground (give or take a protection diode drop), but input levels are just given in terms of logic high or low.
Can someone please tell me the maximum input voltage for a low state (VIL Max), and minimum voltage for a high state (VIH Min), so I can make sure my drive circuit is compatible?
Thanks
Show LessHi,
I want to make a small signal analysis of the BGB707L7ESD. For this s2p files are provided.
In their measurement setup Vbias is decoupled from the RF path. However, in the reference designs of the design guide the Vbias pin is part of the RF matching.
So in order to make a proper simulation one would need a s1p file for that pin or some SPICE model. However, this is not offered by Infineon.
How should I proceed?
Thanks
Georg
Show Less
Is HMC994APM5E a low-noise amplifier, I am unfamiliar with this kind of product. Thanks.
I recently plan to use bgt24ltr11 to measure distance. After I have collected the medium frequency signal, how should I process it to obtain distance information for a stationary target? My transmission method is pulse linear frequency modulation, that is, the VCO is modulated with a sawtooth wave, and it is sent every once in a while. At first, I used the FFT method for echoes to check the spectrum to find the peak value to determine the distance, but in the official demo board, this method is used to measure moving targets, and there is no mention of measuring static targets.
Show LessUsing LNA like the BGA525N6, we are amplifying signals from a Dual Feed patch antenna.
SO as a result after amplication and SAW filters we end up with two signals.
What is available/how to combine these signals to the input into a signal pin on a standard GPS module
Show LessHi, I'm looking for the evaluation board of the LNA BGA9H1MN9. Does anyone know where I can find it? Thank you!
We want to design with Infineon BGA9H1MN9 (Mid- and High-Band Low Noise Amplifier with Gain Steps and MIPI Control) that the data sheet featured follows the MIPI RFFE 2.1 standard. Unfortunately, the datasheet itself did not show the MIPI protocol, formatting, and timing diagram.
I attempted to download the MIPI RFFE 2.1 from mipi.org, but the site won’t allow me to be a member to download it.
We want to interface and access the registers of the BGA9H1MN9 using an FPGA. We need the details on the protocol, formatting, and timing diagram. How and what are the steps to get the MIPI RFFE 2.1 standard? Else, if there is a separate document for the BGA9H1MN9 that details the protocol, formatting, and timing diagram, where can I get that?
Thanks in advance for any help given.
Show LessDoes anyone know where I can download Mipistick.exe, which is the executable f to the Infineon MIPI RFFE Master (mipi stick) software and driver.
Show Less