Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Legacy microcontrollers Forum Discussions

lokesh
Level 1
Level 1
First reply posted First question asked Welcome!

Hi ALL

While dumping my algorithm code in the cypress fm4 board is not dumped. I have not used any header file.

Some flash memory exceeds the size.

I am using keil license version also.

While running some delay code it is working fine. 

Kindly gives me suggestion.

0 Likes
2 Replies
VenkataD_41
Moderator
Moderator
Moderator
750 replies posted 500 replies posted 250 solutions authored

Hi,

Is this happening with only one project or all the projects?

Since you are not using any header file, can you please replace the delay code with your main.c and try to build once? If this step causes errors, can you please attach your main.c file to this thread?

Thanks and regards

Ganesh

0 Likes
lokesh
Level 1
Level 1
First reply posted First question asked Welcome!

HI Ganesh,

Here is the attached main file and error details. I have used the LMS function which is  predefined in the compiler. I used the LMS function and try to pass the parameter. The main file and error is in attachment.

0 Likes