Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Legacy microcontrollers Forum Discussions

Not applicable
Hi,
I’ve a hybrid control unit with a C167 controller, 95320 SPI eeprom and 29F400 flash.
I want to read the SPI eeprom somehow. I tried it by Minimon in bootstarp mode, but I can read the flash only, because if I choose the Minimon driver for the eeprom (X25160), than I can’t see “reas_SPI_eeprom” between the features and I can’t run it.
Has somebody any idea, how to read the eeprom?
Thanks is advance!
Zax
0 Likes
7 Replies
Not applicable
up...
bump...
0 Likes
Not applicable
Zax wrote:
up...
bump...

what do you mean by bump... solve the problem if you can
0 Likes
Not applicable
Bump means I still waiting for useful comments.
For real help I would even pay.
0 Likes
Not applicable
Zax wrote:
Bump means I still waiting for useful comments.
For real help I would even pay.

oh. ok. As I'm new here so asking questions frequently for my knowledge. thanks for information 🙂 by the way me too waiting for useful comments
0 Likes
Not applicable
This is my "board", not a usual PCB. 🙂
I hope, it's interesting enough to help me!
The biggest on the left hand is the C167, right hand side is the 29F400 flash and the smallest in the middle is the 95320 eeprom.
2368.attach
0 Likes
User9698
Level 3
Level 3
Wooooooooooooo!!!!!!!!!!!!!:(
WHAT IS THAT Man???are you ok?
this is very complicated.can you find bootloader pins of this board? {Reset, PL04,RX,TX}?
0 Likes
Not applicable
hemn wrote:
Wooooooooooooo!!!!!!!!!!!!!:(
WHAT IS THAT Man???are you ok?
this is very complicated.can you find bootloader pins of this board? {Reset, PL04,RX,TX}?


As I wrote in the first comment, I already read the flash, so yes, I find all of this pins 🙂
0 Likes