Legacy microcontrollers Forum Discussions
What is the accuracy range of the TC367DP to capture the current of an amplified BLDC?
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/AURIX/%E7%94%B5%E6%9C%BA%E6%8E%A7%E5%88%B6%E8%AF%8A%E6%96%AD/td-p/732038
Show Less
Hello dear infineon frends,
I currently have a problem with the Tricore from Infineon. The controller is currently being used in series production. Some controllers do not start after a reset. When I connect to the debugger/JTAG and execute the debug software reset, the application starts normally. If I do a hardware reset, the controller hangs.
I have compared working controller with the faulty controller. Working controller starts after "Idle mode" → "Normal mode". Faulty controller starts after "Idle mode" → "Sleep mode". Can you perhaps give me a tip on what I should look for? What is the reason for this problem?
Many thanks in advance
Greetings
Alexander
Hello, I am using TLE92464ED chip to output current, I configured the parameters according to the registers but there is no current output, here is my attachment, read is the return value of the chip read. Is there a problem with my register configuration? Or do you have a driver demo for TLE92464ED?
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E4%BC%A0%E7%BB%9F%E5%BE%AE%E6%8E%A7%E5%88%B6%E5%99%A8/TLE92464ED%E8%8A%AF%E7%89%87%E7%9A%84%E4%BD%BF%E7%94%A8/td-p/484127
Show Less Hello, I need your help. Thank you very much
It is normal for the program to jump from the boot area to the app area, but after jumping from the app area to the boot area, the program in the app area does not run normally, and it is looping in one place. The program keeps looping at 0x00C00090.
Now it is certain that the jump instruction is no problem, the program has jumped to the boot area, before jumping I have closed the interrupt. Or provide some code about software reset, I tried software reset, but it failed, maybe my instructions are not correct.
Hi all,
with this post I´d like to understand wether there is a suitable successor for the CYRF69103 chip which has become obsolete.
I´m interested in replacing this chip on one of my projects with a nearly similar one. I already came accross one which has the label CYRF6935. Would this be an option? How long will this one be available on the market?
Looking forwards for one reply.
Thanks in advance,
Martin
Show Less
BTN8982TA The silkscreen doesn't match the specification on the official website, would like to help with this, thanks.
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E7%94%B5%E6%9C%BA%E6%8E%A7%E5%88%B6%E8%8A%AF%E7%89%87/BTN8982TA-%E4%B8%9D%E5%8D%B0%E4%B8%8E%E5%AE%98%E7%BD%91%E7%9A%84%E8%A7%84%E6%A0%BC%E4%B9%A6%E5%AF%B9%E4%B8%8D%E4%B8%8A/td-p/722268
Show LessHello,
i know this is not the correct forum. But i have not found a more suitable one.
I would like to know the difference between the types CY90F543GPFR-GE1 and CY90F543GPF-GE1. I could not find the meaning of "R" in the designation so far.
I don't think it has anything to do with the packaging, as both parts are delivered in the tray.
Thank you very much for your help.
Show LessSAF-XE167F-96F80L AC 需要帮忙解答一下尾缀AC表示什么意思呀?
Hello,
We are currently using an FMx family of microcontrollers, and we are using files provided by Infineon (including the former Cypress).
These include the source code and header files (xxx.c, xxx.h, xxx.inc) of the "microcontroller I/O register declaration file" and "I/O register macro declaration file".
Am I correct in understanding that these do not fall under FOSS (Free Open Source Software)?
Best Regards,
Kawata