Legacy microcontrollers Forum Discussions
As https://community.cypress.com/docs/DOC-15108 description, how much clock rate I can configuration, and What effect will it have?
Show LessWe have plan to used XC2268N, but I can not find XC2268N Dip file for DAVE2.
I confirmed XC2236N, XC2238N, XC2265N in the XC22xxN DIP file.
there is a difference in package between xc2236N(QFP 64) and xc2268N(QFP 100)
there is a difference in CAN node between xc2265N(3 node) and XC2268N(6 node)
How to use XC2268N in the dave2?
How can I get the XC2268N Dip file or another method to used DAVE2 for XC2268N?
Best Regard.
Kwon Show Less
Hello, I am doing my first project with Cypress MCU-I want to communicate with nRF24L01 tranceiver via SPI. I am using CSIO in SPI mode from PDL 2.1.0, but then I try to build the project with Keil I get message ".\output\release\s6e2ccxj_template.axf: Error: L6218E: Undefined symbol PINRELOC_SET_EPFR (referred from main.o)." There were a lot more, but I figured out it was because definitions between .h files were lacking so I managed to solve all errors but this one because I had not found definition of PINRELOC_SET_EPFR so I am asking maybe someone could help with this problem? Maybe I am doing it all wrong? I will add my project file to the post.
Show LessHello,
a customer is asking me to freely change an image Logo through a USB Mass Storage.
I wrote the code to read from the USB Mass Storage, and it works fine.
My problem is to change the Logo image.
Consider that this logo always resides in the very begininng of the HyperFlash (that should be at address 0xC0000000) and that it is a 480x272 pixel 24bpp BMP, so the whole size, including the header, is 391700 bytes (20 bytes for the header and 391680 bytes for the bitmap data).
I tried many examples without success, both from sample codes and from datasheets (for example AN218684).
My hardware and software configuaration is exactly the same as per the FM4-176L-S6E2DH eval board).
Can you suggest me a solution?
Thank you very much in advance
Regards
GianLuca
Show LessI am trying to connect Memtool 4.7 with a XE166 to program it with a new Software.
I do receive always the same error message from memtool:
"Message from component 'IMTMemtool' :
Can't connect to Target
Message from component 'MiniMonTargIntf' :
Failed to create connection failed report !
Message from component 'MiniMonTargIntf' :
Can't connect target !
Message from component 'MiniMonTargIntf' :
Bootstrap loader not responding !
Please check:
- Target power supply
- Communication cable
- Communication settings"
Targetdevice has power and the cable should not be a problem either because its used for other communications without any problem.
The Pin-settings on the board match the specification for connecting with ASC Bootstrap Loader as mentioned in Infineons manuals, the software settings of memtool should be ok, too, but i think they do not come in to play as the error happens before they are used:.
I have watched the data-transmission between PC and Device. Memtool sends a proper zero-byte with start- and ending-bit but the XE166 does not respond with the 0xD5. It´s responding with 0xC9 which might be a problem for memtool because it can´t verify it as correct code and does not have it as error-code either.
Maybe somebody can help and tell what this respond means or where I can find a list of error-respond-codes so I can look my error code up.
Oh, and of course I tried with different boards of the same kind. After the fifth board with the same beavhiour I am pretty sure it is no broken Hardware.
Thanks in Advance.
Edit:
Might be relevant: I tried new boards only Show Less
We are using the MB9BFD18T FM3 microcontroller in our application for which we have started production. (We recently ordered 1,000 OFF from Arrow.)
To program the PCBs in production we are using the FLASH MCU Programmer for FM0+/FM3/FM4.
I am also currently writing an application for testing our PCBs in production, and ideally would like to combine programming and testing into the same application.
To do this, would it possible to obtain the source code for your programmer application? It would be of great help to use this code in our application.
Show LessHi,
I am working on S6J3400 micro. I need to implement RAM and ROM(Flash) and Flash 1-bit and double bit error injection test. Could you please provide RAM and Flash 1-bit and double bit error injection test sample code. Also provide local contact information in INDIA.
Thanks,
Damu
Show LessHello, friends! Where is the error reconstruction flow chart (AN204470 HFI low speed)?
I want create programm for MB91F469G mcu, test some samples. How to get Softune IDE?