Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Legacy microcontrollers Forum Discussions

NaMo_1534561
Legacy microcontrollers
Hello,According to the Errata information in the data sheet of MB9BF102NA, the Errata will be fixed in Rev.A.In this silicon revision, does MB9BF102N ... Show More
gulec_2585086
Legacy microcontrollers
Hello,We found that INITX pin has an internal pull-high, and we can't using the BMC(internal 78K-128K PD) control this pin to low level.Do you know ho... Show More
lihuc_1231266
Legacy microcontrollers
We are automated programming equipment maker. Pegatron is going to program CYSHM35925I. Can you please send us the programming technical documents? Show More
hejic_1412251
Legacy microcontrollers
this code is genarated by USB Wizard,Mass Storage Example.run in SK-FM0-64L-S6E1C3 evaluation board.trace to usb/1533  will go to  HardFault_Handler,w... Show More
neba_3919101
Legacy microcontrollers
Due to  memory constraint, I want to share the common code (example UART code) between bootloader and application. I am using MB95F778 controller. Loo... Show More
User17084
Legacy microcontrollers
Hi .. Anyone have a datasheet for any of those special trace board chips used in Hitex emulators XC2000ED, XC2080ED, XC2090ED ?Is it possible to run a... Show More
Chva_1477726
Legacy microcontrollers
To allI need to know if the FM0+ pins are protected, like the PSoC MCU pins, with the two diode configuration connected to Vss and Vdd.I went through ... Show More
krboc_4116076
Legacy microcontrollers
I am from the Intel Hyderabad India.Issue on windows 10For my project I am using FR Family SOFTUNE Workbench V60L11 to compile and debugging the code,... Show More
Regan_Yan
Legacy microcontrollers
IAR7.8+JLINK遇到这个问题,有什么建议吗? Show More
mavec_1488271
Legacy microcontrollers
Hello,I Read from the datasheet that is possible to connect an SDRAM chip the the S6E2CCA uController, up to 256Mbytes if the packager allows it.Is th... Show More