Legacy microcontrollers Forum Discussions
Anyone have a datasheet for any of those special trace board chips used in Hitex emulators XC2000ED, XC2080ED, XC2090ED ?
Is it possible to run any of those chips in 128Mhz emulate a XC2788 cpu ?
Who is supplying the best R&D tools for the XC2000 controllers ?
Regards
Richard Show Less
To all
I need to know if the FM0+ pins are protected, like the PSoC MCU pins, with the two diode configuration connected to Vss and Vdd.
I went through the >1000page peripheral manual, the TRM and the product manual and could not find any info on it.
Regards
Chris
Show LessI am from the Intel Hyderabad India.
Issue on windows 10
For my project I am using FR Family SOFTUNE Workbench V60L11 to compile and debugging the code, I am trying to connect “MB2100-01A-E Single Port Embedded Emulator Debugger SPEED-BOX” debugger for debugging code, I am not able to connect because of signature driver missing(error message : ***F9417S: The USB driver is not found. "SiDRVo2.dll") on windows 10 laptop, can you please help me to resolve this issue.
Environment used
=> Windows 10 operating system on laptop.
=> FR Family SOFTUNE Workbench V60L11.
=> MB2100-01A-E Single Port Embedded Emulator Debugger SPEED-BOX
=> MB91F526LSB
Issue on windows 7
on windows 7 seeing MB2100-01A-E driver mismatch and not able to update MB2100-01A-E driver, can you please provide MB2100-01A-E driver software and debugger setup process on softune workbench.
please let me know if you required any information.
Thanks,
Krishna.
mail ID:- krishnaiah.bommu@intel.com
Show LessHello,
I Read from the datasheet that is possible to connect an SDRAM chip the the S6E2CCA uController, up to 256Mbytes if the packager allows it.
Is there any recommended part, or any resource available to get started? Like an evaluation kit or a software example?
All i could find is an example on the PDL that speaks about a SV6P1615 but I'm not able to find any information about it.
Thanks,
Marco
Show LessI am using Flash programmer for downloading the *.mhx file into MB95F778 controller. Binary downloads properly and flash verification is also ok .But binary execution does not happen after programming and System doesnot start .But when I program in release mode using softune then it works
Show LessI cannot find the SDK or boot loader source for the Traveo S6J33xx family. Where I find this?
I emailed Cypress support and they told me to post here.
Show LessI am embedded developer. I am using xmc4500 relax kit. I want the code for interfacing lcd display with spi or qspi.
I want to use it for matrix orbital make eve2-70 TPR display which has resistive touch.
I have made source file for that but display isnot going on . Code is messed up.
What i need is for Spi enable , spi write, Spi read buffer, spi read.
Please help. Any example please share it. Show Less
There is little information about this MCU, I need to flash it through RS232 or programmer. So where is the rs232 programmer software? thanks!
Show LessS6J32HELTNSC20000(B1.1)
S6J32GELTNSC20000
Which is the burner corresponding to this chip?
Is there a way that I can quickly find the appropriate burner for any chip,Instead of asking each part number every time
Show Less