Legacy microcontrollers Forum Discussions
Dears.
I'm doing part selection with Traveo 1 S6J329.
Are there anyone who knows the following box (Pink color) ?
Are they related to MultiCAN? If it's possible, I would like to get detail information.
Thanks and Regards,
Wonjin(Kevin) Han
Show LessDears.
My customer is taking into account to use Traveo S6J329 to design HVAC controller for automotive.
They would like to review reference schematic but there is no it on Cypress Web.
I'm wondering that is possible to share reference schemaitc for S6J329.
If it's possible, schemaitc which is implemented and is evaluated in S6J329 EVK is the best for them.
Thanks and regards,
Wonjin Han.
Show LessHi
Does anyone know what the replacement procedure is for MB90F497G.
ie Pin for Pin Compatibility, and including an assembler or software backup, we would even accept Windows XP solutions.
Why is Cypress directing queries for Softune to distributors who cannot supply the software. We would greatly appreciate a legitimate statement/direction regarding the continuity of Fujitsu devices.
Show LessHi Sir,
Now my customer is beginning their project using CY9AF116NAPMC-G-MNE2. Now they have an question in CSV . In PDL , CSV is OFF .
But in 002-05586 Mannual main part , it discribes as flows:
Does the CSV work after starting?
Thanks.
Show LessHi
We need a simple assembler or "Softune" for MB90F497G (the F2MC-LX family)
We need to re-code old designs and flash the existing products.
Please advise on an Assembler strategy if Softune is not available.
Thank you
Show LessWe have been directed to "Cypress Distributors" for IDE's for devices like CY90F497GPFM-G-FLE1 on Digi-Key as well as all the F²MC-8 to 16bit devices
None of the Suppliers can provide assistance.
According to Cypress:
Arrow Electronics
Digi-Key Corporation
Future Electronics
Newark/element14
Mouser Electronics
Verical
RS Components
Will supply the the 8 to 16 Bit Devices, and will provide software support for same.
Do we need to approach the Top Electronics Forums, Fujitsu, and the public platforms of the above companies, for advice and a solution to editing our designs or is there software available for use?
Show LessCan you send me a "Flash mcu programmer for F2MC-16FX" software. As the download in the website does not work. I need to read/write the MCU Flash
Show LessHow to realize DC chopper waveform output function?Pulse with different amplitude of output waveform。The model of single chip computer is S6E1A12B0A。Thank you。
Show LessHello together,
I try to download the flash of an MB90F497G, using F²MC-16LX Software and adn Silicon Labs USB-UART Bridge.
My application has a programming connector, pinned with MD0, MD2, P01, P00, SOT1, SIN1, VCC, GND and SCK1.
MD0 is LOW, MD1 and MD2 High, i meassured, P01 and P00 also low.
Crystal is 8 MHz.
I did not connect SCK1, cause I do not now where.
I get different errors.
Sometimes:
ERROR!! MCU:31H DOWNLOAD ERROR
ERROR!! MCU:02H DOWNLOAD ERROR
And so on. different HEX Numbers as error.
Does anybody know what i am doing wrong?
May anybody help me?
I have not read about code protection at F497G anywhere.
Thank you in advance.
Show LessHowever, I can not find the file “Cfg_PosIf_RdcDs.c” which is required to run the application board with a resolver position sensor.
You can find the reference to this file in the PDF “eMotor application example (PMSM with FOC)” page 13.
Thanks for your help. Show Less