Legacy microcontrollers Forum Discussions
We are design in theS6J334CHEESE20000 devices related to Sambo Motors SPTM project.after the first event, we received a request for AEC-Q100, 101, 200 certification materials from Ssangyong. Please check the following materials and deliver the data.
BR,
Tony Kim
Show LessWhat is the recommended IDE for full featured firmware development? ie code editor, integrated with in-circuit-debugger, realtime step-thru/over/into, local variable watches, etc?
Also what debug hardware is required?
Thanks! Show Less
Hi,
Customer wants PWM output using base timer.
I understand that the following registers should be set.
1)TMCR
2)TMCR2
3)STC
4)STCC
5)STCS
6)PCSR
7)PDUT
8)TMR
I understand the address of each channel as follows.
0xB080_8000 to 0xB080_AFFF (ch0 to ch11)
Is this understanding correct?
Best Regards,
harukawa
Show Lesspls share errata sheet for MB95F778E controller.
Hi,
FM3 CY9B110T Series.
It seems like UART max baud rate is 8MHz, Why isn't it 14.4 MHz?
In the document 'FM3 Peripheral Manual Communication Macro Part (TRM)',
following formula is shown.
V = φ/ b - 1
V : Reload value
b : Baud rate
φ: Bus clock frequency or external clock frequency
CY9B110T Series APB2 Bus clock is max 72MHz and V is min 4.
Even considering the allowable baud rate range for reception,
Maximum baud rate is..
b = φ/( V + 1 ) = 72 Mhz / ( 4+1 ) = 14.4Mhz ( baud rate max )
However, in the data sheet it is 8 MHz.
(※Document History 03/09/2017 Added the Baud rate spec in “12.4.10 CSIO/UART Timing”)
■CY9B110T Series, 32-bit Arm® Cortex®-M3 based Microcontroller Datasheet
https://www.cypress.com/file/252801/download
■32-bit Microcontroller FM3 Peripheral Manual Communication Macro Part
https://www.cypress.com/file/211101/download
Why is this?
Is it because the specification of MFT needs 8 clocks
for setting the interrupt flag by checking the reception idle status?
Is there any other reason?
Best regards.
Shimoda
Show LessAre there bootloader & bootloadables for the FM0+? I could not find any info and no component available in PSoC creator. I need the firmware to be field upgradable through a serial port.
Any support will be welcomed.
Regards
Chris
Show Less初めまして、JOHNAN(株)の平島と申します。
Cypress FM4に関して、以下の質問をお願い出来ますでしょうか?
【質問】
①Keil社のMDK-ARM5での開発は可能でしょうか?
②STM社のHALライブラリのライブラリはありますか?
③STM社のTouchGFXのようなタッチパネル開発ツールはありますか?
以上。
よろしく、お願いします。
Show Less