Legacy microcontrollers Forum Discussions
I'm after a BSDL file that will work for the XE169FH LQFP176 CMS, any help would be appreciated.
Regards
Hari
I use a design with an xc2000 controller and recently buy a mini wiggler v3 tools because i wanna make some debugging on my application.
After some problems to adapt OCDS 20 pins to the JTAG interface , i sucessfully connected my board to DAS server and under Tasking VX.
My main problem at this point is i can not achieve debugging of C code.
I can program and run my application but when i try to add a breakpoint on the c code that s said me that i can not put a breakpoint here ( every where give the same result),
When i put a sbrk assembler instruction, the program stop and the diassembly window appears
When i put the program is pause, dissamssembly windows appears too...
Others strange points are , depending of debug configuration, the debugger should stop a 1rst instruction of man function, this behavior never appears : /
So Is it possible to debug C code with a miniwigglerV3 or i need a tantino debugger to make it ?
Thanks for help
SC. Show Less
Hi,
Unable to install Serial Port Viewer and Terminal (v.5.8.3) for Windows 10 64bit for the FM4-176L-S6E2CCA-ETH Pioneer Kit. The download window comes up for a fraction of a second, then the screen turns into what you see in the attachment. I am unable to accept terms and download in time. I have tried for several days on multiple computers and different browsers. I had no problems installing the PDL and CMSIS-DAP files. What is going on?
Thanks
David
Show Less
Hi
May I know what are states of S6E1A11B0AGP20000 X0 and X1 pins if they are floating?
The customer measured X0 and X1 pins' voltages and got 1.3-1.5V when the board's powered. Is that right ?
Thanks.
BR
Grace
Show Lessパラレルプログラマーモードでデバイスを書き込みたいんですが、
どこからパラレルプログラマー仕様書をダウンロードすることが可能でしょうか?
I'm thinking of using the ISO1H816G integrated in my project, but I couldn't find any documents about SPI communication. What value do I need to send to the integrated SPI to activate pins via SPI? Show Less
Dear Madam/Sirs,
Please advise me of difference among following CY90F497GPMC products.
CY90F497GPMC-GE1
CY90F497GPMC-GSE1
CY90F497GPMC-G-FLE1
CY90F497GPMC-GS-FLE1
Thank you for your cooperation.
Best regards,
Takuya Hase / Altima, Macnica, Inc.
Show LessDear community,
I search for a solution to program an MB96F34x IC with command line tool. I already have the Flash.exe program:
but I need a way to run this program (or a similar program) in command line with the necessary arguments (like mhx filename, com port, tartget MCU, adresses, etc.).
Example:
C:\>flash.exe cmd --port="COM3" --target="MB96F346R" --freq=4 --start=FD0000 --end=FFFFFF -full filename.mhx
Could anybody help me in this issue?
Thanks in advace,
Gabor
Show Less御担当者様
CY90F598GPF-GE1 終息方向、
↓
Next Best Alternative Part:CY90F598GDPF-GSE1
とのことで、上記赤文字部分のPackage情報(差異)を頂きたく存じます。
後継品のデータシートが見つけられなかったため。
宜しくお願い致します。
小島
Show LessDear Madam/Sirs,
Please confirm and advise if the difference among following MPNs are only memory size?
Also please advise if they can be replaceable.
If there is any other difference feature than memory size, please kindly advise.
S6E2C18H0AGV2000A
S6E2C19H0AGV2000A
S6E2C1AH0AGV2000A
Thank you for your cooperation.
Best regards,
Takuya Hase / Altima, Macnica, Inc.
Show Less