Legacy microcontrollers Forum Discussions
Hi,
I want to make a BOOT code and have some questions about the jump function and the link footer address assignment. If you have any reference demos, please provide them, preferably IAR engineering.
thanks
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E4%BC%A0%E7%BB%9F%E5%BE%AE%E6%8E%A7%E5%88%B6%E5%99%A8/%E8%AF%B7%E9%97%AE%E6%9C%89%E6%B2%A1%E6%9C%89S6J324%E5%8F%AF%E4%BE%9B%E5%8F%82%E8%80%83%E7%9A%84BOOT-APP%E4%BB%A3%E7%A0%81/td-p/677821
Show LessHello, I have equipment using the C167CS microcontroller and I want to copy its programming to put on another similar device, but I don't know how to do that!
Which program can read and write and which pins will be used?
please guide me
thanks
is in a tractor transmission module.
Show LessFor a customer of us we need to place the SAK-C505CA. The controller needs to be programmed before production and I was wondering if there is an SMD IC mount availiable that we could place on the PCB and afterwards mount the microcontroller.
Show Lesssmartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/MEMS%E9%BA%A6%E5%85%8B%E9%A3%8E/MEMS%E9%BA%A6%E5%85%8B%E9%A3%8E/td-p/677286
Show LessHello, how do I define a variable to a specified RAM address? For example, define the i variable at RAM address 0x0200, thank you!
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E4%BC%A0%E7%BB%9F%E5%BE%AE%E6%8E%A7%E5%88%B6%E5%99%A8/softune-%E5%A6%82%E4%BD%95%E6%8A%8A%E4%B8%80%E4%B8%AA%E5%8F%98%E9%87%8F%E5%AE%9A%E4%B9%89%E5%9C%A8%E6%8C%87%E5%AE%9A%E5%9C%B0%E5%9D%80/td-p/673835
Show LessHello, Infineon China support. I would like to ask a question. When I was developing this 92104, I first raised the ENA pin and then started SPI to send the dog feed. It seemed to enter FAIL SAFE mode. Did I clear GENSTAT first, then feed the dog, then ban the dog??
Also, when you first raise the ENA pin, do you have to wait 150uS to send SPI??
I wonder if there is an official flowchart or the like to easily support development??
Best wishes, thank you
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E7%94%B5%E6%9C%BA%E6%8E%A7%E5%88%B6%E8%8A%AF%E7%89%87/%E5%85%B3%E4%BA%8ETLE922104%E7%9B%B8%E5%85%B3%E7%8A%B6%E6%80%81%E6%B5%81%E7%A8%8B%E5%9B%BE/td-p/676803
Show Lesssmartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E7%94%B5%E6%BA%90%E7%AE%A1%E7%90%86%E8%8A%AF%E7%89%87/3PCS01G-%E7%8E%B0%E5%9C%A8-%E8%BE%93%E5%85%A5%E7%94%B5%E6%B5%81%E6%B3%A2%E5%BD%A2%E5%9C%A8%E9%A1%B6%E9%83%A8%E5%92%8C%E5%BA%95%E9%83%A8%E6%9C%89%E7%95%B8%E5%8F%98%E7%9A%84%E6%83%85%E5%86%B5-%E8%AF%B7%E9%97%AECOMP%E8%84%9A%E5%A6%82%E4%BD%95%E5%81%9A%E4%BC%98%E5%8C%96/td-p/676356
Show LessHello. We are using 3PCS01G to design the PFC part of the charger. There is a situation where the PFC MOS breaks down after a period of use, so it is better to replace the PFC MOS.
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E7%94%B5%E6%BA%90%E7%AE%A1%E7%90%86%E8%8A%AF%E7%89%87/3PCS01G-PFC%E7%94%B5%E8%B7%AF%E5%87%BA%E7%8E%B0%E5%AE%A2%E6%88%B7%E7%AB%AF%E4%BD%BF%E7%94%A8%E4%B8%80%E6%AE%B5%E6%97%B6%E9%97%B4%E5%90%8E%E5%9D%8FPFCMOS/td-p/672873
Show LessHello everyone, which agent can support CY9BF121JPMC-G-JNE2
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E4%BC%A0%E7%BB%9F%E5%BE%AE%E6%8E%A7%E5%88%B6%E5%99%A8/CY9BF121JPMC-G-JNE2/td-p/673501
Show LessHello everyone, which agent can support CY9BF121JPMC-G-JNE2
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E4%BC%A0%E7%BB%9F%E5%BE%AE%E6%8E%A7%E5%88%B6%E5%99%A8/CY9BF121JPMC-G-JNE2/td-p/673502
Show Less