Legacy microcontrollers Forum Discussions
Manual says they should be found in the datasheet but so far I have been unable to find the lock/unlock values for the AXI and AHB MPUs. Does anybody know them?
Show LessI am using SBC (tle9273) as the slave which communicates to RH850F1KHD8 microcontroller (Master) through SPI communication.
When I send a command through SPI, MISO and MOSI data are improper even if SCL and CS signal are proper when probed through CRO.
I am using the following configurations as per my slaves requirement
1. SPI FIFO mode selected
2. SPI LSB first
3. SPI Mode1 used for communication
4. Port Muxing are corrected as per my hardware.
5. The Baudrate of SPI is 2MHz
Please guide me on how to configure the SBC in Normal mode. Also please provide me any sample code available for SBC Tle9273 for configuring it.
Thanks in advance. Show Less
Hello,
I've bought a FM4-176L-S6E2GM board and successfully run the board example projects.
Now I would like to modify the s6e2gm_I2S_hp in order to continually stream a a buffer using interrupts instead.
I got some code from the i2s_irq_play_wave_via_wm8731 project in the PDL example folder.
First I had to change &I2cCh to MFS1_I2C1 to successfully Initialize WM8731 via I2C.
The interrupt callback however is called only once so after the first fifo buffer is transmitted nothing more happens.
Can someone point to the error ? The code is attached
Thanks
john
Show LessPosted materials related to the setting of registers, etc. of the CY96640 series to the following community.
It is a continuation of this inquiry.
https://community.cypress.com/message/221211#221211
On the cypress page, you can refer to the errata material of the F2MC-16FX Programming Manual (CM44-00203-3).
=> https://www.cypress.com/file/237411/download
Would you provide us with the F2MC-16FX Programming Manual (CM44-00203-3)?
*
If you search for "CM44-00203-3" in the search (Google), you can find the original version of the material.
=> https://www.fujitsu.com/downloads/MICRO/fma/mcu/prog16fx-cm44-00203-3e.pdf
Is there a Cypress version of this document?
Best Regards,
Harukawa
------------------------------------------
CY96640シリーズのレジスタ等の設定に関する資料について、下記コミュニティでやり取りさせて頂きました。
これの続きの問い合わせです。
https://community.cypress.com/message/221211#221211
cypressページでは、F2MC-16FX プログラミングマニュアル(CM44-00203-3)のエラッタ資料が参照できます。
=> https://www.cypress.com/file/237411/download
F2MC-16FX プログラミングマニュアル(CM44-00203-3)について、提供頂けないでしょうか。
※
検索(Google)で"CM44-00203-3"で探すと、開発元版の資料が見つかります。
=> https://www.fujitsu.com/downloads/MICRO/fma/mcu/prog16fx-cm44-00203-3e.pdf
これのCypress版資料がございませんでしょうか。
以上、よろしくお願い致します。
春川
Show LessHello.
My customer wish to use a HyperBUS RAM.
The S6J329C has a HyperBUS ch.1, ch.2 and a HS-SPI for a graphic core.
Can it use a Hyper BUS ch.2 with a HS-SPI FLASH(G_SLK0, G_CS, G_DQ0, G_DQ1, G_DQ2, G_DQ3) for a graphic core?
The HS-SPI flash uses the 0x4000 0000 address. the HyperBUS RAM 0x4800 0000.
Can it use as above?
Thanks and Best regards.
Glenn.
Show LessI am trying to automate a process that include loading a new program into de TriCore board, run it for a a while and them load a new program.
But after loading a new program TriCore needs an reset, which we want to automate.
Is there a way to send a reset signal via CLI using any of the Aurix Tools, in order to automate the process?.
Or any other recommendation to achieve that objective?.
Thanks in Advance
euw15 Show Less
Hi,
I've been trying to connect to the Traveo S6J334EJT, with no success. I am aware that I need to specify the core type as Cortex-R5 in a script so I have done so. I am using the Segger Flasher ARM with the latest version of the software to do this.
I have attached the .log file from the Flasher.
Anyone have any ideas?
Thanks,
Mark
Show LessIn macro SetPinFunc_SINX_Y and similar there appear two numbers (X and Y) If I understand well the first number is the serial channel, what is the function of the second one ?
Show LessHi,
I'm looking for materials related to the setting of registers, etc. of the CY96640 series.
The CY96640 series hardware documentation can be found on the Cypress page, but no technical reference manual documentation for the software is found.
Is there a technical reference manual for the software?
Best Regards,
Harukawa
---------
CY96640シリーズのレジスタ等の設定に関する資料を探しています。
CY96640シリーズのハードウェア資料はCypressページから参照できますが、
ソフトウェアに関するテクニカルリファレンスマニュアル資料が見つかりません。
ソフトウェアに関するテクニカルリファレンスマニュアル資料がありませんか。
以上、よろしくお願い致します。
春川
Show Less