Legacy microcontrollers Forum Discussions
text.format{('custom.tabs.no.results')}
Hi,
客户是win7 64bit系统,直接安装驱动很困难,让客户全部卸载之后,直接安装softune 3021版本,成功安装驱动,但后来又安装了一款离线烧写器驱动之后,MB2146-07无法正确连接,重新安装驱动也不能用,但是设备管理器里显示MB2146-07正常,实际上无法连接仿真器。重新安装softune3021也不行,请问这种情况如何解决?谢谢!
Show Less
Hi All,
This is Madhusoodana Bairy from Mistral Solutions, Bangalore.
We are in need of 4 Lane or 2 Lane LVDS to CSI Converter Chip.
Whether the company supports this kind of chipset or any low end CPLDs/FPGAs which will do this job ?
Thanks.
Best Regards,
Madhusoodana Bairy
Show LessDear Cypress:
After checked the 32-bit_Microcontroller_FM3_Peripheral_Manual_Main_Part_TRM.pdf , we can't find the detail discription, can you help to provide ? tks'
Show LessI have recently bought an STM32 Nucleo-64 G474RE. I want to use this MCU for Field-Oriented Control (FOC or Vector Control) with a BLDC motor. I have seen there are many libraries available and
there is the ST Motor Control Workbench tool available. But I am confused as to which tool and/or library. I should use with this board. I have never done FOC before but I know theory behind it and I would
like to, at least, develop a program using the resources available. Please your help would be really appreciated. Also would the Motor Control Workbench be compatible with my MCU ? (I have no motor
or powerboard at my disposal due to the quarentine). Your help would be really appreciated. Show Less
Q.
I want to drive a three-phase brushless motor (one) and a brush motor (two) using CY9BF524L.
For example,
I think it can be realized by using a multi-function timer (PPG timer:3ch) for the brushless motor and using PWM (2ch) for the brush motor.
Is this understanding correct?
Best Regards,
Harukawa/TED
---------------------------------------------------
Q.
CY9BF524Lを使って三相ブラシレスモータ(1つ)とブラシモータ(2つ)を駆動させたい。
例えば、
ブラシレスモータは多機能タイマ(PPG:3ch)を使用し、
ブラシモータをPWM(2ch)を使うことで実現できると思います。
この理解は正しいですか。
Show LessI'm having the following error:
Error[Li005]: no definition for "Mfs_Uart_Init" [referenced from C:\Users\rcorder1\Documents\IAR Embedded
Workbench\GPIO & ADC\arm\8.50.1\Cypress\s6j3200\S6J3260Evl\examples\adc12b\single_irq_sw\TCFLASH
Debug\Obj\main.o]
Error[Li005]: no definition for "Mfs_Uart_Write" [referenced from C:\Users\rcorder1\Documents\IAR Embedded
Workbench\GPIO & ADC\arm\8.50.1\Cypress\s6j3200\S6J3260Evl\examples\adc12b\single_irq_sw\TCFLASH
Debug\Obj\main.o]
Error[Li005]: no definition for "Mfs_Uart_Read" [referenced from C:\Users\rcorder1\Documents\IAR Embedded
Workbench\GPIO & ADC\arm\8.50.1\Cypress\s6j3200\S6J3260Evl\examples\adc12b\single_irq_sw\TCFLASH
Debug\Obj\main.o]
Error while running Linker
I'm trying to "merge/combine" the ADC and UART examples for Cypress s6j3200
Using Windows 10, IAR Arm 8.50.1
Build log:
Show Less
Building configuration: single_irq_sw - TCFLASH Debug
Updating build tree...
Linking
ilinkarm.exe C:\Users\rcorder1\Documents\IAR Embedded Workbench\GPIO & ADC\arm\8.50.1\Cypress\s6j3200\
S6J3260Evl\examples\adc12b\single_irq_sw\TCFLASH Debug\Obj\adc12b.o C:\Users\rcorder1\Documents\IAR
Embedded Workbench\GPIO & ADC\arm\8.50.1\Cypress\s6j3200\S6J3260Evl\examples\adc12b\single_irq_sw\
TCFLASH Debug\Obj\exceptions.o C:\Users\rcorder1\Documents\IAR Embedded Workbench\GPIO & ADC\arm\
8.50.1\Cypress\s6j3200\S6J3260Evl\examples\adc12b\single_irq_sw\TCFLASH Debug\Obj\flash_marker.o C:\
Users\rcorder1\Documents\IAR Embedded Workbench\GPIO & ADC\arm\8.50.1\Cypress\s6j3200\S6J3260Evl\
examples\adc12b\single_irq_sw\TCFLASH Debug\Obj\interrupts.o C:\Users\rcorder1\Documents\IAR Embedded
Workbench\GPIO & ADC\arm\8.50.1\Cypress\s6j3200\S6J3260Evl\examples\adc12b\single_irq_sw\TCFLASH
Debug\Obj\main.o C:\Users\rcorder1\Documents\IAR Embedded Workbench\GPIO & ADC\arm\8.50.1\Cypress\
s6j3200\S6J3260Evl\examples\adc12b\single_irq_sw\TCFLASH Debug\Obj\mfs_uart.o C:\Users\rcorder1\
Documents\IAR Embedded Workbench\GPIO & ADC\arm\8.50.1\Cypress\s6j3200\S6J3260Evl\examples\adc12b\
single_irq_sw\TCFLASH Debug\Obj\pdl.o C:\Users\rcorder1\Documents\IAR Embedded Workbench\GPIO & ADC\
arm\8.50.1\Cypress\s6j3200\S6J3260Evl\examples\adc12b\single_irq_sw\TCFLASH Debug\Obj\port.o C:\Users\
rcorder1\Documents\IAR Embedded Workbench\GPIO & ADC\arm\8.50.1\Cypress\s6j3200\S6J3260Evl\examples\
adc12b\single_irq_sw\TCFLASH Debug\Obj\start.o C:\Users\rcorder1\Documents\IAR Embedded Workbench\
GPIO & ADC\arm\8.50.1\Cypress\s6j3200\S6J3260Evl\examples\adc12b\single_irq_sw\TCFLASH Debug\Obj\
startup.o C:\Users\rcorder1\Documents\IAR Embedded Workbench\GPIO & ADC\arm\8.50.1\Cypress\s6j3200\
S6J3260Evl\examples\adc12b\single_irq_sw\TCFLASH Debug\Obj\sysctrl.o C:\Users\rcorder1\Documents\IAR
Embedded Workbench\GPIO & ADC\arm\8.50.1\Cypress\s6j3200\S6J3260Evl\examples\adc12b\single_irq_sw\
TCFLASH Debug\Obj\Traveo_template_version.o --no_out_extension -o C:\Users\rcorder1\Documents\IAR
Embedded Workbench\GPIO & ADC\arm\8.50.1\Cypress\s6j3200\S6J3260Evl\examples\adc12b\single_irq_sw\
TCFLASH Debug\Exe\single_irq_sw.out --redirect _Printf=_PrintfFullNoMb --redirect _Scanf=_ScanfFullNoMb --map
C:\Users\rcorder1\Documents\IAR Embedded Workbench\GPIO & ADC\arm\8.50.1\Cypress\s6j3200\S6J3260Evl\
examples\adc12b\single_irq_sw\TCFLASH Debug\List\single_irq_sw.map --config C:\Program Files (x86)\IAR
Systems\Embedded Workbench 8.4\arm\config\linker\Cypress\s6j33xDx.icf --semihosting --entry
__iar_program_start --vfe --text_out locale
IAR ELF Linker V8.50.1.245/W32 for ARM
Copyright 2007-2020 IAR Systems AB.
Error[Li005]: no definition for "Mfs_Uart_Init" [referenced from C:\Users\rcorder1\Documents\IAR Embedded
Workbench\GPIO & ADC\arm\8.50.1\Cypress\s6j3200\S6J3260Evl\examples\adc12b\single_irq_sw\TCFLASH
Debug\Obj\main.o]
Error[Li005]: no definition for "Mfs_Uart_Write" [referenced from C:\Users\rcorder1\Documents\IAR Embedded
Workbench\GPIO & ADC\arm\8.50.1\Cypress\s6j3200\S6J3260Evl\examples\adc12b\single_irq_sw\TCFLASH
Debug\Obj\main.o]
Error[Li005]: no definition for "Mfs_Uart_Read" [referenced from C:\Users\rcorder1\Documents\IAR Embedded
Workbench\GPIO & ADC\arm\8.50.1\Cypress\s6j3200\S6J3260Evl\examples\adc12b\single_irq_sw\TCFLASH
Debug\Obj\main.o]
8'058 bytes of readonly code memory
1'214 bytes of readonly data memory
3'390 bytes of readwrite data memory
Errors: 3
Warnings: none
Link time: 0.08 (CPU) 0.06 (elapsed)
Error while running Linker
Total number of errors: 3
Total number of warnings: 0
Build failed.
I am using MB96F388HSBPMC-GE2 MCU in one of our project. I want to know what will happen exactly (or what will be the impact) if I use a 1 uF ceramic capacitor as smoothing capacitor at C pin instead of the datasheet recommended minimum value of 3.5 uF?
Thanks.
Show LessPlease release the CY95F012KPFT-G-UNE2 datasheet