Legacy microcontrollers Forum Discussions
text.format{('custom.tabs.no.results')}
I am currently working with a FlexRay Evaluation Kit (https://www.fujitsu.com/downloads/MICRO/fma/pdfmcu/app_ug-910011-15-flex-fpga-eva-kit-369.pdf ). Does anyone know how to use the gateway program? Should it just work when two boards are connected, how do I tell if it is working?
Thanks,
Show Lesssomebody know how to configure ADC2 CH 8
or Do we have some errata sheet for ADC TLE983x
or sample code ...?
thanks in advance
Br sajan Show Less
Hello,
I am working with the FM4-176L-S6E2CC-ETH Starter Kit and the IAR embedded workbench IDE. I would like to use the serial timer function of the MFS Channels in CSIO mode (found that in the communication manual and in the PDL drivers), but I can not set any of the registers. Now i am wondering if this feature is maybe not available at all with my MCU.
More information:
MFS Channel 4, sending and transmitting works fine, same for setting interrupt and FIFO config.
All the relevant register values (CSIO_SACSR etc.) are shown as 0xFFFF
Thanks in advance for your help.
Show LessI'm currently working with a s6j32hel board, but since IAR (v 8.50) doesn't have that device i configured it with s6j32gel.
When a click 'Download and debug' it gives me the following warnings, how can this be fix?
Debug Log:
Show Less
Mon Apr 06, 2020 11:19:39: IAR Embedded Workbench 8.50.1 (C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.4\arm\bin\armproc.dll)
Mon Apr 06, 2020 11:19:39: Loaded macro file: C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.4\arm\config\debugger\Cypress\S6J3200.dmac
Mon Apr 06, 2020 11:19:39: Loaded macro file: C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.4\arm\config\debugger\Cypress\TRAVEO_DEBUG.dmac
Mon Apr 06, 2020 11:19:39: Loaded macro file: C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.4\arm\config\flashloader\Cypress\FlashS6J3xx_TC128KB_S384KB.mac
Mon Apr 06, 2020 11:19:39: Loading the I-jet driver
Mon Apr 06, 2020 11:19:39: Probe: Probe SW module ver 1.65
Mon Apr 06, 2020 11:19:39: Probe: Option: trace(Auto,size_limit=25%)
Mon Apr 06, 2020 11:19:39: Probe: Found I-jet, SN=88726
Mon Apr 06, 2020 11:19:39: Probe: Opened connection to I-jet:88726
Mon Apr 06, 2020 11:19:39: Probe: USB connection verified (11538 packets/sec)
Mon Apr 06, 2020 11:19:39: Probe: I-jet, FW ver 7.2, HW Ver:B
Mon Apr 06, 2020 11:19:39: Probe: IJET-ARM20 adapter detected
Mon Apr 06, 2020 11:19:39: Probe: Versions: JTAG=1.85 SWO=1.40 A2D=1.73 Stream=1.50 SigCom=2.44
Mon Apr 06, 2020 11:19:39: Emulation layer version 4.61
Mon Apr 06, 2020 11:19:39: JTAG clock detected: 12MHz
Mon Apr 06, 2020 11:19:39: JTAG chain "TDI->TAP#1[IR=5]->TAP#0[Cortex:IR=4]->TDO" verified.
Mon Apr 06, 2020 11:19:39: Notification to init-after-power-up hookup.
Mon Apr 06, 2020 11:19:39: Notification to core-connect hookup.
Mon Apr 06, 2020 11:19:39: Connected DAP on JTAG. Detected DP ID=0x0.
Mon Apr 06, 2020 11:19:39: Connecting to TAP#0 DAP APB-AP port 1 (IDR=0x24770002) to core Cortex-R5 r1p3 at 0x80090000.
Mon Apr 06, 2020 11:19:39: Debug authentication:
Mon Apr 06, 2020 11:19:39: Non-secure invasive debug not implemented
Mon Apr 06, 2020 11:19:39: Non-secure non-invasive debug not implemented
Mon Apr 06, 2020 11:19:39: Secure invasive debug enabled
Mon Apr 06, 2020 11:19:39: Secure non-invasive debug enabled
Mon Apr 06, 2020 11:19:39: Debug resources: 8 H/W breakpoints, 8 watchpoints, 1 context ID breakpoints.
Mon Apr 06, 2020 11:19:39: CPU status OK
Mon Apr 06, 2020 11:19:39: LowLevelReset(script, delay 200)
Mon Apr 06, 2020 11:19:39: Calling reset script: ResetAndStopAtEndOfBootROM
Mon Apr 06, 2020 11:19:39: ----- Prepare hardware for flashloader -----
Mon Apr 06, 2020 11:19:39: Disabling Caches...
Mon Apr 06, 2020 11:19:39: Configuring and initializing TCRAM (128KB)...
Mon Apr 06, 2020 11:19:39: Initializing System RAM (384KB)...
Mon Apr 06, 2020 11:19:40: Clear WDT
Mon Apr 06, 2020 11:19:40: Loaded debugee: C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.4\arm\config\flashloader\Cypress\FlashS6J3xx_TC128KB_S384KB.out
Mon Apr 06, 2020 11:19:40: Target reset
Mon Apr 06, 2020 11:19:41: Unloaded macro file: C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.4\arm\config\flashloader\Cypress\FlashS6J3xx_TC128KB_S384KB.mac
Mon Apr 06, 2020 11:19:41: Downloaded C:\Users\rcorder1\Documents\IAR Embedded Workbench\Template 3200\arm\8.50.1\Cypress\s6j3200\S6J3260Evl\examples\template\TCFLASH Debug\Exe\template.out to flash memory.
Mon Apr 06, 2020 11:19:41: 4272 bytes downloaded into FLASH (2.20 Kbytes/sec)
Mon Apr 06, 2020 11:19:41: Loaded macro file: C:\Users\rcorder1\Documents\IAR Embedded Workbench\Template 3200\arm\8.50.1\Cypress\s6j3200\S6J3260Evl\examples\template\..\..\config\tcflash.mac
Mon Apr 06, 2020 11:19:41: Disabling MPU and Caches...
Mon Apr 06, 2020 11:19:41: Loaded debugee: C:\Users\rcorder1\Documents\IAR Embedded Workbench\Template 3200\arm\8.50.1\Cypress\s6j3200\S6J3260Evl\examples\template\TCFLASH Debug\Exe\template.out
Mon Apr 06, 2020 11:19:41: LowLevelReset(software, delay 200)
Mon Apr 06, 2020 11:19:41: Calling reset script: SoftwareReset
Mon Apr 06, 2020 11:19:41: LowLevelReset(script, delay 200)
Mon Apr 06, 2020 11:19:41: Calling reset script: ResetAndStopAtEndOfBootROM
Mon Apr 06, 2020 11:19:41: 4272 bytes verified (245.40 Kbytes/sec)
Mon Apr 06, 2020 11:19:41: Download completed and verification successful.
Mon Apr 06, 2020 11:19:41: LowLevelReset(software, delay 200)
Mon Apr 06, 2020 11:19:41: Calling reset script: SoftwareReset
Mon Apr 06, 2020 11:19:41: Target reset
Mon Apr 06, 2020 11:19:41: INFO: Configuring trace using 'Auto,size_limit=25%' setting ...
Mon Apr 06, 2020 11:19:41: Trace: Using detected ETMv3 at address 0x8009c000
Mon Apr 06, 2020 11:19:41: Trace: ETMv3 is not powered-up (ETMCR=0x441)
Mon Apr 06, 2020 11:19:41: Trace: ETMv3 powered-up OK (ETMCR=0xc40)
Mon Apr 06, 2020 11:19:41: Trace: Access to detected ETMv3(architecture=3.3) initialized (CONF=0x8d254024, CTRL=0xc40, IDR=0x4104f230)
Mon Apr 06, 2020 11:19:41: Trace: Using detected ETB at address 0x80001000, RAM size 0x1000 words (16KB)
Mon Apr 06, 2020 11:19:41: Trace: Configured as 'ETMv3 to ETB' (SW ver: Trace2=1.33 ETM=1.00 ETB=1.05 Deco=1.42)
Mon Apr 06, 2020 11:19:41: Could not measure 'ITrgPwr' when ETM/ETB mode is active.
Mon Apr 06, 2020 11:19:41: There was 1 warning during the initialization of the debugging session.
Mon Apr 06, 2020 11:19:41: The stack pointer for stack 'SVC_STACK' (currently 0x00000018) is outside the stack range (0x00000A00 to 0x00000A80)
Mon Apr 06, 2020 11:19:41: The stack pointer for stack 'IRQ_STACK' (currently 0x00000020) is outside the stack range (0x00000A80 to 0x00000B00)
Mon Apr 06, 2020 11:19:41: The stack pointer for stack 'FIQ_STACK' (currently 0x00000028) is outside the stack range (0x00000B00 to 0x00000B80)
Mon Apr 06, 2020 11:19:41: The stack pointer for stack 'UND_STACK' (currently 0x00000008) is outside the stack range (0x00000B80 to 0x00000C00)
Mon Apr 06, 2020 11:19:41: The stack pointer for stack 'ABT_STACK' (currently 0x00000010) is outside the stack range (0x00000C00 to 0x00000C80)
I write a Bootloader for a FM4 CY9BF368 with the Standard Frequenz of 160 MHz.
After I change the Program counter
_asm("LDR PC, [R0, #4]"); //Load new program counter address
the Firmware doesn't start if it is compiled with the Frequenz of 8MHz.
If the Frequenz of the Firmware are change to 160 MHz it works.
Here are the different Settings at System_mb9b360r.h
CLOCK_8MHZ
APBC0_PSR_Val ( 0x00000000ul)
APBC2_PSR_Val ( 0x00000080ul)
SCM_CTL_Val ( 0x0000002Aul)
CLOCK_160MHZ
APBC0_PSR_Val ( 0x00000001ul)
APBC2_PSR_Val ( 0x00000081ul)
SCM_CTL_Val ( 0x00000052ul)
What going wrong ?
Can I change the Frequenz during the lifetime of the bootloader before I jump to the Firmware ?
Thanks,
Harald
Show LessHello, ALL
I am a new student, I need the MB9D560 SDK package.
Who help me? thank you !
I need the MB9D560 SDK, include the software driver and example.
I need the EVB board, How can I buy it.
Show LessWhat is the difference between the errors in Softune:
Invalid communication status( or cable connection). "(11)"
and
Invalid communication status( or cable connection). "(17)"
Thanks
Show Less