Legacy microcontrollers Forum Discussions
Hi All,
I'm looking for recommended Flash Writer/Programmer for F²MC . (MB95F128JBPMC)
Current Writer is NET IMPRESS AF320(Yokogawa).
Please tell me recommended Flash Writer/Programmer Products/Parts#
------------------------
F2MCの推奨の書き込み機を探しています
既存はNET IMPRESS AF320です
そのほかに推奨の書き込み機があれば教えてください
Show Lessan204470 document for hfi low speed how can fined example base this document
Can yocto linux be used on xmc4500 relax kit for gui project?
Hello.
It's about four items from the Cypress product portfolio (pls see them listed below) - I know at least one (CY96F348HSCPMC-GSE2) is under EOL status - but I can't find anything related to the other three.
My question: are there specific discontinuation plans for those four items or will Infineon continue to manufacture them? Or are there replacements on Infineon´s end?
My customer has requirements of approx. 100k p.a. and if possible he want to avoid a re-design and is interested in long-term-availibility.
Thx a mil
Ulrich
CY90F342CASPFR-GSE1
CY96F338RSAPMC-GS-UJE2
CY91F467BAPMC-GS-UJE2
CY96F348HSCPMC-GSE2
Show LessI am working on a new project, using SAF-XC167CI-32F40F BB-A mcu. For simulating purposes I will be needing an IBIS model of this device. Does anyone had experienced a similar issue, and if so, how he has went thru it ?
Also , it could not be exactly the same MCU, mentioned above, but an IBIS model of a close in parameters MCU would help also a lot.
Thanks! Show Less
S6J328CL has 1-channel 4-bit x2 DDR HSSPI. I want to connect to it external QSPI Serial Flash ROM (S25FL128S or S25FL256S), for reading images to be displayed via graphic subsystem.
In datasheet "6.1 Port Description List" (p.62-63) 8 data pins and 2 select pins HSSPI are mentioned twice: in role Graphic HSSPI and role MCU HSSPI. The fundamental difference in the clock pins (G_SCLK0 - 74 pin, M_SCLK0 - 65 pin). See image (pin overlap - green, pin differences - red😞
One more moment: In hardware manual "1. Memory Map" (p.64-65) memory for HSSPI mapping in two area: Graphic subsystem (4000_0000 - 4FFF_FFFF) and CPU (8000_0000 - 8FFF_FFFF).
Do I understand correctly, that clock in flash memory in my case should be connected to G_SCLK0 Graphic HSSPI?
Does the choice (of G_SCLK0 and M_SCLK0) affect which memory area the data will be mapped to?
I need to choose a debugger/flash programmer for controller XC161CJ and i think miniwiggler should do this , so i have below given questions :
1. will it work with memtool to flash load the software
2. to flash load the software what all files are required (e.g. .hex file ), if i purchase miniwiggler hardware debugger
3. Will it work with tasking EDE ver (C166/ST10v8.0.r1) for debugging purpose (will it take the symbol file ? from IDE?)
4. How to connect miniwiggler to 16 pin connector.
5. Will miniwiggler able to access and flash the memory area on different chip also?
Thanks
sanjyot Show Less
I am using TLE9879 evaluation board. I want to put RTOS on this board. I checked but there is no sample code available with free RTOS. Please tell me configuration of Free RTOS. or is any demo example available Show Less