Legacy microcontrollers Forum Discussions
Hi,
we need to call the FLASH MCU Programmer tool by using the command line.
we tested with following command:
flash.exe "MB9BF524K/L/M" 4MHz test.mhx COM12 dialog
But nothing happens, except at txt File gets generated in the install directory of the FLASH MCU Programmer that contains:
NG
No.101 Please set "hex file"
We are using the Version V01,L16 of the FLASH MCU Programmer.
Kind Regards, Michael
Show LessHi,
Kindly let me know where can I find ibis model of S6E2CCAL0AGL2000A.
I'm looking for a BSDL file that will work for the package PAB416 (416 pin BGA) of the microcontroller CY91F528Y 32-bit FR81S. For the purpose of developing boundary scan tests in the final product.
Regards.
AB
Show LessDears.
Is QSPI supported on S6E1C series?
Thanks and Regards.
Hi,
I want to develop an SW for XE167F-96F device, but as I can c it uses the Keil c166 compiler. Can I also use GCC compiler to build the SW or can I port the SW so that it can be built using GCC compiler?
Thanks,
Vishal
Show LessHi,
I have been trying to get the SPI working on a XC2734 chip to read a eeprom.
Problems i have is with receiving the data, the RBUF always stays 0x00 and never changes.
Check data with a scope and on the MISO input line i see data and it is changing on different address reads.
But RBUF always returns 0x00.
P10.0 Data input MISO
P10.1 Data output MOSI
P10.2 Clock
P10.8 CS
void EEPROM_test()
{
char recValue = '0';
U0C0_PCRL = 0x0F4F;
P10_OMRH = 0x0100; // P10.8 CS Output Low
U0C0_SCTRH = 0x071F; // Sets frame length on 4 byte
vSendData1(0x03);
vSendData1(0x01);
vSendData1(0xD0);
vSendData1(0xFF);
recValue = uwGetData();
//recValue = U0C0_RBUF;
P10_OMRH = 0x0001; // P10.8 CS Output High
}
void vSendData1(uword uwData)
{
U0C0_TBUF00 = uwData; // load transmit buffer register
while(!(U0C0_PSR & 0x1000)); // wait until tx buffer indication flag is set
U0C0_PSCR |= 0x1000; // clear transmit buffer indication flag
}
uword uwGetData(void)
{
while(!((U0C0_PSR & 0x8000) || (U0C0_PSR & 0x4000)));
U0C0_PSCR |= 0xC000; // clear alternate receive indication flag & receive indication flag
return U0C0_RBUF; // return receive buffer register
}
HI
Is it possible to some programming specification for MB91F59BCPB-GSE1?
Thanks
Peter
Hello.
I found the different between clock in datasheet and clock in Platform Part manual.
<datasheet>
<Platform Part Manual>
Why are the max values different?
Thanks and Best regards.
Glenn.
Show Less