Legacy microcontrollers Forum Discussions
We met with a problem about the connection between the chip and DAS. The chip we use is XC2224L, VQFN package. DAP connector of DAP miniwiggler. The schematic refers to the Easy Kit XC2XXX. The DAS can not recognize the chip. Memtool 4.4 was also tested but failed.
Already connect 'TDO_A' to 470R then GND and '/TRST' to 2.74K to +5V.
While connecting, 'RESET' is high. '/PORST' is high.
Do you have any idea about that?
Thanks. Show Less
I am using A7670C GSM breakout board with an ESP32.
Connections
- RX-TX
- TX-RX
- GND-GND
I am giving external power to the GSM module, 3.8 V according to the product description.
When I sent the AT command to GSM module, I don't get output on the serial monitor of the Arduino IDE.
The message is sent to a particular number successfully, but I don't receive the message from mobile.
This is my code:
I'm trying to write a short code for TC1796 CPU but I've faced an issue.
When I use the following assembler code everything works fine:
call 0x800xxxxx
ret
But the following code does not work and I have no clue why:
movh.a a15, #High
lea a15, [a15]Low
nop // tried without this instruction also
calli a15 // crushed
ret
I hope that Infineon engineers can shed light on this problem. When I replace calli to call(only this single instruction) the code works just fine. So I believe the problem with "CALLI" instruction.
Hi~
Im wondering whether CY96610 Series( ex : CY96F612RBPMC-GS-UJE1) has ASIL rating or not.
Also, Im looking for whether it has HSM in it or not.
Many thanks
BRs
Show Less Hello, I need your help. Thank you very much
It is normal for the program to jump from the boot area to the app area, but after jumping from the app area to the boot area, the program in the app area does not run normally, and it is looping in one place. The program keeps looping at 0x00C00090.
Now it is certain that the jump instruction is no problem, the program has jumped to the boot area, before jumping I have closed the interrupt. Or provide some code about software reset, I tried software reset, but it failed, maybe my instructions are not correct.
Hi all,
with this post I´d like to understand wether there is a suitable successor for the CYRF69103 chip which has become obsolete.
I´m interested in replacing this chip on one of my projects with a nearly similar one. I already came accross one which has the label CYRF6935. Would this be an option? How long will this one be available on the market?
Looking forwards for one reply.
Thanks in advance,
Martin
Show Less
BTN8982TA The silkscreen doesn't match the specification on the official website, would like to help with this, thanks.
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E7%94%B5%E6%9C%BA%E6%8E%A7%E5%88%B6%E8%8A%AF%E7%89%87/BTN8982TA-%E4%B8%9D%E5%8D%B0%E4%B8%8E%E5%AE%98%E7%BD%91%E7%9A%84%E8%A7%84%E6%A0%BC%E4%B9%A6%E5%AF%B9%E4%B8%8D%E4%B8%8A/td-p/722268
Show LessHello,
i know this is not the correct forum. But i have not found a more suitable one.
I would like to know the difference between the types CY90F543GPFR-GE1 and CY90F543GPF-GE1. I could not find the meaning of "R" in the designation so far.
I don't think it has anything to do with the packaging, as both parts are delivered in the tray.
Thank you very much for your help.
Show LessHi Infineon.
MB9B110T and CY9B100A have min and max value of smoothing capacitor in recommended operating conditions.
(Min value is 1uF and max value 10uF.)
Please confirm recommended operating conditions of below link.
MB9B110T DS:
CY9B100A DS:
https://www.digikey.jp/htmldatasheets/production/1867767/0/0/1/mb9b100a-series.pdf
But, there is no description of min and max value of smoothing capacitor in MB9B160R(CY9BF166NPMC-GNE2) datasheet.
Please confirm recommended operating conditions of below link.
Could you please let us know min and max value of smoothing capacitor for MB9B160R(CY9BF166NPMC-GNE2)?
Best Regards.
YuMa
Show LessSAF-XE167F-96F80L AC 需要帮忙解答一下尾缀AC表示什么意思呀?