Recent discussions
Hello,
I am working with the FM4-176L-S6E2CC-ETH Starter Kit and the IAR embedded workbench IDE. I would like to use the serial timer function of the MFS Channels in CSIO mode (found that in the communication manual and in the PDL drivers), but I can not set any of the registers. Now i am wondering if this feature is maybe not available at all with my MCU.
More information:
MFS Channel 4, sending and transmitting works fine, same for setting interrupt and FIFO config.
All the relevant register values (CSIO_SACSR etc.) are shown as 0xFFFF
Thanks in advance for your help.
Show LessHello, ALL
I am a new student, I need the MB9D560 SDK package.
Who help me? thank you !
I need the MB9D560 SDK, include the software driver and example.
I need the EVB board, How can I buy it.
Show Lessワークフラッシュを「セクタ消去一時停止」、「セクタ消去再開」するサンプルコードはありますでしょうか。
ここにあるProgramming Specificationを参照し、
「セクタ消去一時停止」および「セクタ消去再開」を試みましたが、動作いたしません。
消去コマンド書き込み直後に消去一時停止のみを実行すると、不定値(例:08, 0C)が書き込まれていた。
消去コマンド書き込み直後に消去一時停止→一時停止再開を実行すると、同じ不定値でセクタは20秒経っても消去されませんでした。
オペレーションの問題なのか、基板設定の問題なのかわからず、まずはFW側できちんと消去できるかを試したいです。
よろしくお願いします。
Show LessI am try reading data status register from flash W25N01GVZEIG TR, logic analyzer show that all ok
but i am getting 0xFF. Receive works in interupt mode, code: https://godbolt.org/z/MbGacj
What i am doing wrong. Show Less
To all,
I have place a Windows PC terminal source code in C# on the Code sharing forum.
PC Terminal Program with C# Source Code
Enjoy,
Len
Show LessI write a Bootloader for a FM4 CY9BF368 with the Standard Frequenz of 160 MHz.
After I change the Program counter
_asm("LDR PC, [R0, #4]"); //Load new program counter address
the Firmware doesn't start if it is compiled with the Frequenz of 8MHz.
If the Frequenz of the Firmware are change to 160 MHz it works.
Here are the different Settings at System_mb9b360r.h
CLOCK_8MHZ
APBC0_PSR_Val ( 0x00000000ul)
APBC2_PSR_Val ( 0x00000080ul)
SCM_CTL_Val ( 0x0000002Aul)
CLOCK_160MHZ
APBC0_PSR_Val ( 0x00000001ul)
APBC2_PSR_Val ( 0x00000081ul)
SCM_CTL_Val ( 0x00000052ul)
What going wrong ?
Can I change the Frequenz during the lifetime of the bootloader before I jump to the Firmware ?
Thanks,
Harald
Show LessHow does it mean this surface printing ?
Model : MB9BF124LPMC1-G-JNE2
Surface printig : 1625 326
1625 = 2016 / 25W ?
326 = ?
マイコンのシルク印刷表記について、下記は何を表しているのでしょうか?
型格:MB9BF124LPMC1-G-JNE2
印刷:1625 326
⇒1625:16年25週?
326:?
Show Less您好!
我在网站上看到softune的链接,
上面说找local sales或者发起一个technical support case来得到下载链接,我找了local sales好像很难找到,因此到这里来发起一个 technical support case, 希望能够给我一个下载链接。
谢谢!
chester
Show Less