Legacy microcontrollers Forum Discussions
How to improve the problems of traditional microcontrollers such as lack of response time and low reliability of controllers in harsh environments? Thanks.
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E4%BC%A0%E7%BB%9F%E5%BE%AE%E6%8E%A7%E5%88%B6%E5%99%A8/%E4%BC%A0%E7%BB%9F%E5%BE%AE%E6%8E%A7%E5%88%B6%E5%99%A8%E5%AD%98%E5%9C%A8%E7%9A%84%E9%97%AE%E9%A2%98/td-p/733492
Show LessI opened up the head unit from our vehicle and realised I could turn the screen into a very versatile little monitor. The reason for its retirement was because the touch screen stopped working… You can ask at the Automotive shops that do installations or the Wreckers for your own head units, the LCD can still be good even if the touchscreen glass was cracked (use an inferior MCU to run it instead and have a spare Cypress chip). Mine is the LSP2GTS (a.k.a. Anatel 52098606), it has only two video inputs, one split to go to both chips (termination resistor halved).
Chip list includes:
AU1340 Micropr (with two 1Gbit RAM W971GG6JB, 32G flash JW983 and 64Mbit s29gl064n90)
TW8816 flat panel processor (with 800x480 LB070WV1-TD05; five inputs)
TW9900 video decoder (four more inputs)
CY8C21334-24PVXA touch sensing microprocessor
SAF7741HV audio DSP (TEF7000HN one radio tuner; fourteen inputs (see fig 2, 31))
70F3351GC(A)SG3 microprocessor (near DSP) no idea, sound synthesis?
RBFA C211C Bluetooth
I was entertaining thoughts of using a PIC 12C508 (or something reusable) and emulate I2C to activate the TW8816's OSD and program to show the Composite, S-Video, Component (analogue and digital), and RGB (analogue and digital) inputs (and read their configuration)- until I saw what the touchscreen was controlled with. Likely the Cypress failed due to extensive environmental heating (poorly positioned), I am not sure if the OEM's (it is LG and Holden(General Motors) branded) code can be extracted🖊️ and fixed, if so can add my stuff around it, and send touches to my code. The OSD programming won't take much room even if I do a good job at it (and i could add extracurricular activities in the OSD interface, like forwarding I²C commands and MCU pin commanding, could port some 16 colour games to show on the OSD). The AU1340 could be lost technology so not bothering with that (there is an 8bit XIP MCU in the TW as well). I wasn't going to bother with the DSP, twice the codeing. I see you would you start accessing the chip using MiniProg1, MiniProg3 or ICE-Cube. Is it possible to use another microcontroller instead just like you can use PICs to program PICs🖊️? I have never done microprocessors before (since circuits can blink LEDs cheaper), I am happy with assembly but so far Cypress downloading is difficult (maybe they dislike Android, and their staff don't do website troubles).
Show LessDears.
I'm looking for the information about " How much MIPS (million instructions per second) it has ?"
Please review it and give me your feedback.
Thanks and best regards,
Wonjin Han.
Show LessHello,
Please tell me how to handle the pins when the FM3 clock pins (X0A, X1A) are not used.
Due to the hardware configuration these pins cannot be set to GPIO.
I am assuming that perhaps the X1A pin should be open and X0A should be pulled down, is this correct?
If so, what is the appropriate value for the pull-down resistor?
--
Shimamura
How to set the interrupt source of each core for TC277 inter-core communication? CPU0 interrupt source is 0, CPU1 is 4, CPU2 is 8. I don't know if this is the right setting.
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E4%BC%A0%E7%BB%9F%E5%BE%AE%E6%8E%A7%E5%88%B6%E5%99%A8/TC277%E6%A0%B8%E9%97%B4%E9%80%9A%E4%BF%A1%E6%AF%8F%E4%B8%AA%E6%A0%B8%E7%9A%84%E4%B8%AD%E6%96%AD%E6%BA%90%E5%BA%94%E8%AF%A5%E6%80%8E%E4%B9%88%E8%AE%BE%E7%BD%AE/td-p/732043
Show Less
Hello dear infineon frends,
I currently have a problem with the Tricore from Infineon. The controller is currently being used in series production. Some controllers do not start after a reset. When I connect to the debugger/JTAG and execute the debug software reset, the application starts normally. If I do a hardware reset, the controller hangs.
I have compared working controller with the faulty controller. Working controller starts after "Idle mode" → "Normal mode". Faulty controller starts after "Idle mode" → "Sleep mode". Can you perhaps give me a tip on what I should look for? What is the reason for this problem?
Many thanks in advance
Greetings
Alexander
Hello, do you have any suggestion for replacement material for these two ICs?
1, CY7C924ADX-AXC
2, CY7C924ADX-AC
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E4%BC%A0%E7%BB%9F%E5%BE%AE%E6%8E%A7%E5%88%B6%E5%99%A8/Cypress-IC-8B10B-Conversation-Replacement-Proposal/td-p/719062
Show LessHello, I am using TLE92464ED chip to output current, I configured the parameters according to the registers but there is no current output, here is my attachment, read is the return value of the chip read. Is there a problem with my register configuration? Or do you have a driver demo for TLE92464ED?
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E4%BC%A0%E7%BB%9F%E5%BE%AE%E6%8E%A7%E5%88%B6%E5%99%A8/TLE92464ED%E8%8A%AF%E7%89%87%E7%9A%84%E4%BD%BF%E7%94%A8/td-p/484127
Show LessWe met with a problem about the connection between the chip and DAS. The chip we use is XC2224L, VQFN package. DAP connector of DAP miniwiggler. The schematic refers to the Easy Kit XC2XXX. The DAS can not recognize the chip. Memtool 4.4 was also tested but failed.
Already connect 'TDO_A' to 470R then GND and '/TRST' to 2.74K to +5V.
While connecting, 'RESET' is high. '/PORST' is high.
Do you have any idea about that?
Thanks. Show Less