Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Legacy microcontrollers Forum Discussions

HDTHAS
Legacy microcontrollers
Dear All,  Do Infineon supports SW Crypto Library Ed25519/RSA algorithms for XC2298 Microcontroller ? If Yes where can i find the Crypto Library avail... Show More
Anonymous
Legacy microcontrollers
Hello,all. I am a newbie to here, and I have a question about microcontroller and microprocessor to be solved. I am not quite good at electronics, so ... Show More
ramakrishnanvij
Legacy microcontrollers
Hi,     Can someone point me to the ASC bootstrap loader document for XC167CI-16F40F legacy microcontroller? Thanks, Ram. Show More
lh-f1
Legacy microcontrollers

We are currently using the SAK-XC2267M-104F80LR AB. Is there a suggested alternative in the newer product lines for this?

Fayne_Meng
Legacy microcontrollers

您好,

    我这边需要CY9AF114MAPMC-G-MNE2和CY95F698KPMC1-G-UNE2的Marking Format资料,请提供一下,谢谢。

ShYa_3490236
Legacy microcontrollers
Hi,  In the hardware maunal, pg, 821;”Change the UMask bit while Init bit of the CAN control register (CTRLR) is "1" or while MsgVal bit is "0".” https://www.infineon.com/dgdl/Infineon-MB91580M_S_Series_32-bit_Microcontroller_FR_Family_FR81S_Hardware_Manual_TRM-AdditionalTechnicalInformation-v02_00-EN.pdf?fileId=8ac78c8c7d0d8da4017d0f9356990092... Show More
SuSh_1535366
Legacy microcontrollers

Hello,

I am looking for MB89031A datasheet, but I can't find it.
Please provide me the datasheet.

Regards,
Shimamura

User20074
Legacy microcontrollers
I'm debugging on the basis of the TC1797 controller. As a result of the debugger crash, the controller was in the RESET state. "RESET_TC.001 SCU_RSTST... Show More
Hybridegearbox
Legacy microcontrollers

Can some one tell how to read TC171 tricore please thank you 

CarlKo
Legacy microcontrollers
Dear Please help me find the difference between the two products ** CY91F467DAPFVS vs CY91F467DBPVSR There are no differences in the data sheet Thank... Show More