Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Legacy microcontrollers Forum Discussions

Anonymous
Legacy microcontrollers
XC878 UM 1.1 states in section 4.4:[quote="XC878 UM 1.1"]The Flash Timer has 2 operating modes, Program Timer and Erase Timer modes, whichare selectab... Show More
Ted
Legacy microcontrollers
Has anyone compared software execution time between XC16x and XC2000 with same system clock?

If yes, how was your result?
Anonymous
Legacy microcontrollers
I'm using the D-Flash on the XC878-16FF with 64k Flash. There I have to switch to code bank 2 (MEX1=2) to run functions from XRAM or the Boot ROM.Beca... Show More
Anonymous
Legacy microcontrollers
Hello,I want to interface XC164 with incremental encoder.I red datasheet.It is possible by GPT1.The port of GPT1 is also JTAG/OCDS.How can I use the G... Show More
Anonymous
Legacy microcontrollers
Hello all,For the XC836 devices the default BMI (Boot Mode Index) is "UART BSL Mode". So BMI = 0x00.But when the chip is factory mounted on top of an ... Show More
Anonymous
Legacy microcontrollers
I have two EASY KIT XC836-TSOP boards. One works fine. The other seems to malfunction. So I would like to return the malfunctioning one back into the ... Show More
Anonymous
Legacy microcontrollers
I'd like to do more fine grained interrupt masking, such as only setting EADC = 0 while reading from the variable my ISR stores the conversion result ... Show More
Anonymous
Legacy microcontrollers
Hello,We use XC888 for educational purposes. Today, one of my students tried to use an extarnal interrupt (external interrupt1). To our amazement the ... Show More
Phil
Legacy microcontrollers
Hello,Is there an evaluation kit or demo board available, showing DALI connectivity or the general capability of DALI support from an Infineon Microco... Show More
Anonymous
Legacy microcontrollers
Recently we discovered that the DAP miniWiggler doesn't operate if the empty pins are connected to ground. I always thought they are not connected. Ob... Show More