Legacy microcontrollers Forum Discussions
text.format{('custom.tabs.no.results')}
Hello!
I'm developing FM4-176L-S6E2CC-ETH and knowing there is a standalone example project that Demonstrate LwIP on FM4. However, I'd like to know if there is a way to combine the this project (LwIP over Ethernet Driver) to PDL 2.1? If so, please kindly let me know what should I do to merge them?
http://www.cypress.com/documentation/software-and-drivers/demonstrate-lwip-fm4-sk-fm4-176l-s6e2cc
Thanks.
Tony
Show LessFMシリーズのテンプレートプロジェクトに入っているファイルに関して教えてください。
mb9afaaxn_template-v12.zipを展開すると下記のファイルが生成されます。
+-common-+-base_types.h
| +-mb9aaa0n.h
| +-system_mb9afaax.c
| +-system_mb9afaax.h
+-example-+-ARM-+-....
| | +-....
| +-IAR-+-....
| | +-....
| +source-+-main.c
| +-mcu.h
+-svd-MB9AFAAxN.xml
このうち、「base_types.h」「MB9AFAAxN.xml」の必要性について教えてください。
「base_types.h」はPDL使用時に参照されそうですが、それ以外にどのようなソフトウェア使用するのでしょうか。
「MB9AFAAxN.xml」はヘッダファイル生成に使われそうですが、ユーザが使用するファイルでしょうか。
これらのファイルの必要性について教えて頂けませんでしょうか。
Show LessHi Tech Team,
My name is Praveen Babu, working in Calsonic Kansei north America as s technical specialist.
iam working on HVAC domain. we are using microcontroller MB91F525K.
Iam trying store data in a particular location in RAM from arrays.
When i check in memory map in debug mode, data is not storing in mentioned address in RAM location.
Can u give suggestion how to store data from array of variables in a particular location in RAM.
Show Less
I am a bit new with the infineon microcontroller. I am working on XE169H. I am trying to use the limit check property with the ADC ( only activate an interrupt if the analog input is out of the limits) . I have used Dave to generate the code and I have played around the code with the help of manual but it doesn't work at all.
Here is my code in the attached file.
Any help is welcomed
Kind regards Show Less
Hello everybody,
my Real Time Clock (RTC) on the S6E2DH5J0A works well.
Now I want to set up a 1-second-interrupt.
After clearing all interrupt flags, enabeling the 1-second-interrupt and enabeling (and clearing) the NIVC, the RTC_IRQHandler (void) will be executed immediately.
Moreover it is not possible to return from the RTC_IRQHandler, although I have cleared every interrupt flag and the NIVC.
Did someone have the same problem? Can someone post some code example for setting up the 1 second interrupt of the RTC?
PS: I use FreeRTOS on my MCU.
Show LessThank You Show Less
hello, I porting the firmware on http://www.cypress.com/applications/home-appliances/inverter-fan-motor to MB9BF121K, but motor can not startup.
my questions:
1. can this FW used on MB9BF121K?
2. In this FW, there is a file named Customer_Interface.c, could you give me some documents to disscuss these parameters?
3. Could you give me some other advice?
thanks a lot.
Show LessDear Cypress support team,
Our company works in the ISP field and we build our own programmers and related drivers for programming devices.
I am working with a TRAVEO S6J329C and I am facing some problems.
I have created a small firmware for the device in order to erase, read and program both TCFLASH and WORKING FLASH.
When I chip-erase one of the memories, the first time I read the memory content the values are not correct: as first byte I read 0x00 instead of 0xFF. If I perform again the read operation I get the correct value 0xFF. This appens for every address I try to read, so it is independent from the memory region I try to access. I read from the memory accessing to it by using an *((volatile unsigned char *) pointer using AXI_FLASH addresses.
Using the same firmware but on a S6J32GE device I don't face the same issue.
Is there something that I am missing? The fact is that I would like to read the correct values from the memory from the first access, without having to do a "fake" read just to get rid of the first wrong byte.
Thank you all in advance.
Show LessSK-MB9DF125-001
SK-MB9DF120-001
Hello everyone
I need 2 development boards, please help me. Thank you.
Who do you have this item?
I need
I can buy at a very high price
Please help me.
thank you all
Show Less