What is the pre-programmed BMI and/or USER-ID value for the KIT_XC836_EK ?

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Not applicable
Hello all,

For the XC836 devices the default BMI (Boot Mode Index) is "UART BSL Mode". So BMI = 0x00.

But when the chip is factory mounted on top of an KIT_XC836_EK (Easy Kit), then an "Alarm Clock" example application is pre-programmed in order to have a nice out-of-the-box experience.
I guess that in such pre-programmed Easy Kit chip also the BMI is pre-programmed.

Can anybody disclose what BMI and/or USER-ID values are pre-programmed by Infineon in the XC836 on the KIT_XC836_EK ???

Looking forward to the reply.

Best regards from the chilly Netherlands, Johan.
0 Likes
2 Replies
ysta_4686741
Employee
Employee
Welcome! First question asked First reply posted
The BMI mode pre-programmed for the KIT_XC836_EK is User Mode (Diagnostic) with SPD pin SPD_0. The BMI value is 0x50 and /BMI value is 0xAF.
0 Likes
Not applicable
Dear YS,

Yes, that's precisely what I needed to know. And it works...!!!

Thanks for assisting me.

Best regards from the Netherlands.

Johan.
0 Likes