Not applicable
Apr 09, 2015
11:40 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Apr 09, 2015
11:40 AM
Hi all,
I have an XE167FH controller and want to program the following:
1: /ESR0: The reset function of /ESR0 disablen.
2: /ESR2 as reset out signal with reset out delay after power up. /ESR2 are configured after start up as normal input pin, Pull-up device activated. These Pin can be used together with an external Pull down to hold the signal at a low level. Later in the application software the pin can be switched to Push-pull output driving a high level, at the end of system init (similar to AP16103 chapter 4.2 from Infineon).
Many thanks for your help.
I have an XE167FH controller and want to program the following:
1: /ESR0: The reset function of /ESR0 disablen.
2: /ESR2 as reset out signal with reset out delay after power up. /ESR2 are configured after start up as normal input pin, Pull-up device activated. These Pin can be used together with an external Pull down to hold the signal at a low level. Later in the application software the pin can be switched to Push-pull output driving a high level, at the end of system init (similar to AP16103 chapter 4.2 from Infineon).
Many thanks for your help.
0 Replies