Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Shiozaki
Level 1
Level 1
5 sign-ins First question asked Welcome!

最近PC新しいものに変えたのですが、

新しいPCでSoftuneのオンチップデバッガ(SPEED BOX)を実行すると、

Softuneが落ちてしまう現象が発生しています。

Softuneのバージョンは「F2MC-16 Family Softune Professional Pack (Rev.300027)」です。

 

尚、下記リンクの質問で同様の質問がされていましたので参考にさせて頂き、

USBドライバのバージョン等を確認したところ、バージョンは問題ありませんでしたが、

MB2100-01のプロパティ>「全般」>「デバイスの状態」の欄に

“このデバイスに必要なドライバーのデジタル署名を検証できません。ハードウェアまたはソフトウェアに最近加えられた変更により、正しく署名されていないファイルや破損したファイルがインストールされた可能性があります。また、出どころ不明な悪意のあるソフトウェアであることも考えられます。(コード52)”

という記載があった為、少し気になりました。

https://community.infineon.com/t5/Knowledge-Base-Articles/SOFTUNE%E3%83%AF%E3%83%BC%E3%82%AF%E3%83%9...

どういったことが不具合の原因で、解決方法をご存じでしたら教えて下さい。

宜しくお願い致します。

 

0 Likes
1 Solution
Takashi_M
Moderator
Moderator
Moderator
1000 replies posted 500 solutions authored 750 replies posted

申し訳ございませんが、Softune オンチップデバッガ 起動不良 に一本化させていただきます。

ご理解の程よろしくお願いいたします。

 

View solution in original post

0 Likes
2 Replies
zzz_3221081
Level 5
Level 5
25 solutions authored 100 sign-ins 10 likes received

First, I used a web translator  to read this question.
I don't speak Japanese, nor can I read Kanji.

But to the topic:
Softune is not supported anymore, I think for almost a decade now.
And so are most probably the PC drivers for the debug interface.
Most probably, the drivers were written for a much earlier OS version (Windows), and current OS versions don't support it anymore.
You could perhaps try with different compatibility settings (in File Explorer, context menu).
Or try to run it on a PC with an older OS.

My suspicion is, there will be no update or newer driver.
Many proprietary Fujitsu MCUs are already obsolete, and the rest will probably follow soon.

I am using a debugger from an European company, which uses a generic serial interface (USB-to-serial converter).
(This one : https://www.euros-embedded.com/products/development-environment/symbolic-debugger)
Although there is no support for the F2MC-16 MCU as such, only the debugger.

0 Likes
Takashi_M
Moderator
Moderator
Moderator
1000 replies posted 500 solutions authored 750 replies posted

申し訳ございませんが、Softune オンチップデバッガ 起動不良 に一本化させていただきます。

ご理解の程よろしくお願いいたします。

 

0 Likes