Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Hello,

   

 

   

I wanted to ask on the what is the difference of this IC which is made by FUJITSU and Cypress?

   

How can i program this MCU's by RS232C or JTAG?

   

If there is any special cable used, what is it?

   

I tried to flash it using Cypress Flash USB Direct Programmer. When flashing, it says success, when i checked its not working. 

   

I do use Superpro programmer and it was working, but for some reason USB flashing could be fast and easy.

   

 

   

Any ideas?

   

 

   

Thanks

   

Rey

0 Likes
1 Solution
bharadhwajas_91
Employee
Employee
First like received First like given

Hi

   

What is the hardware you are using ?

   

http://www.cypress.com/documentation/application-notes/an203277-fm-32-bit-microcontroller-family-har...

   

Section 9 explains the hardware connections required , you can also refer the same in chapters 3,4 in the User manual of  FLASH USB DIRECT Programmer.

View solution in original post

0 Likes
2 Replies
Anonymous
Not applicable

this forum is dead?

0 Likes
bharadhwajas_91
Employee
Employee
First like received First like given

Hi

   

What is the hardware you are using ?

   

http://www.cypress.com/documentation/application-notes/an203277-fm-32-bit-microcontroller-family-har...

   

Section 9 explains the hardware connections required , you can also refer the same in chapters 3,4 in the User manual of  FLASH USB DIRECT Programmer.

0 Likes