Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
MaKi_350451
Level 5
Level 5
Distributor - TED (Japan)
250 sign-ins First comment on KBA 10 likes given

Customer is considering their design by S6E2H16F0AGV20000.

They need 160MHz for core clock.

Form below this datasheet, they are considering below two setting.

http://www.cypress.com/file/222996/download

#1. input clock 4MHz, (K=1, N=40, M=2)

#2. input clock 16MHz, (K=1,N=10, M=2)

If both input clock of x'tal are same precision, do you have any differ points between #1 and #2 setting?

(Which is better?)

Thank you & Regards,

Masaya

1 Solution
Anonymous
Not applicable

Hi Kitahora-san,

Sorry for the delayed response.

There is no difference in term of satisfying Spec of the datasheet for both settings.

In terms of which is better, 16 MHz input is preferable.

As 16 MHz reduces the multiplier number, the Band width of the PLL becomes wider, and noise is suppressed, and it becomes advantageous for Jitter characteristics.

Regards,

Nada

View solution in original post

0 Likes
1 Reply
Anonymous
Not applicable

Hi Kitahora-san,

Sorry for the delayed response.

There is no difference in term of satisfying Spec of the datasheet for both settings.

In terms of which is better, 16 MHz input is preferable.

As 16 MHz reduces the multiplier number, the Band width of the PLL becomes wider, and noise is suppressed, and it becomes advantageous for Jitter characteristics.

Regards,

Nada

0 Likes