Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

ryko_3280246
Level 1
Level 1
5 questions asked First reply posted First question asked

Hello,

What happens if erase FMV and FRV Vectors on MB91460 mcu family?

can they be restored?

1 Solution
Praveen
Community Manager
Community Manager
Community Manager
5 likes given 250 sign-ins 100 sign-ins

As mentioned, FMV cannot be erased. What does they mean with they don’t get ACK response from the BootROM? The BootROM is providing a simple internal bootloader in case BSV1/BSV2 have no valid data programmed. If BSV1/BSV2 have valid data, the internal bootloader is skipped and no communication can be done via the internal bootloader. In that case a user software must already be programmed which is communicating via an interface (like a CAN bootloader) in order to re-program or to erase the Flash. If this software is not present in the Flash, the Flash can only be erased by a parallel Flash programmer

Cheers
Praveen

View solution in original post

0 Likes
3 Replies
Praveen
Community Manager
Community Manager
Community Manager
5 likes given 250 sign-ins 100 sign-ins

Please check MB91F460 TRM. In chapter 53 (Fixed Mode-Reset Vector) it is mentioned that these two vectors are independent from the flash and cannot be erased. This means that in internal vector mode (MD[2:0]), after reset the BootROM is always  executed at address 0xBFF8.

Additional information:

By default the user program entry address is set to Flash address 0xF4000. This can be changed by the boot security vectors BSV1 (0x148004) and BSV2 (0x14800C) in order to set a new entry address and to skip the internal bootloader managed by the BootRom (see also figure 53.2-2).

Cheers
Praveen
0 Likes
ryko_3280246
Level 1
Level 1
5 questions asked First reply posted First question asked

When I deleted the sector that contains Fixed Mode Vector and Fixed Reset Vector, and I tried write the new data in this sector, the processor stuck off.

Since then, bootROM never started, I don't get ACK response from bootROM.

0 Likes
Praveen
Community Manager
Community Manager
Community Manager
5 likes given 250 sign-ins 100 sign-ins

As mentioned, FMV cannot be erased. What does they mean with they don’t get ACK response from the BootROM? The BootROM is providing a simple internal bootloader in case BSV1/BSV2 have no valid data programmed. If BSV1/BSV2 have valid data, the internal bootloader is skipped and no communication can be done via the internal bootloader. In that case a user software must already be programmed which is communicating via an interface (like a CAN bootloader) in order to re-program or to erase the Flash. If this software is not present in the Flash, the Flash can only be erased by a parallel Flash programmer

Cheers
Praveen
0 Likes